NXOpen.UF.Drf.AskVerticalNote¶
-
Drf.
AskVerticalNote
()¶ Refer to UF_DRF_ask_vertical_note for documentation.
Signature:
AskVerticalNote(note)
Parameters: note (Tag) – Tag of the note. Returns: Orientation of the note: True if the note is vertical False if the note is horizontal If the object is not a note, False is returned. Return type: bool License requirements: None