WorkpieceBuilderWorkPieceType Enumeration¶
NXOpen.Tooling.WorkpieceBuilder.WorkPieceType is an alias for NXOpen.Tooling.WorkpieceBuilderWorkPieceType
-
class
NXOpen.Tooling.
WorkpieceBuilderWorkPieceType
¶ Bases:
object
the unit type includes the work piece create method
Enum Members
Enum Member Enum Member Description UserDefinedBlock The method defines the block by userCavityCore The method adds the standards of cavity and coreCavityOnly The method adds the standards of cavityCoreOnly The method adds the standards of cavity-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-