WorkpieceBuilderMethodType Enumeration¶
NXOpen.Tooling.WorkpieceBuilder.MethodType is an alias for NXOpen.Tooling.WorkpieceBuilderMethodType
-
class
NXOpen.Tooling.
WorkpieceBuilderMethodType
¶ Bases:
object
the unit type includes the work piece define method
Enum Members
Enum Member Enum Member Description DistanceAllowance Create block by define the distance allowanceReferencePoint Create block by define the reference pointSketch Create block by extrude the sketchKfBox Create block by define the kf box-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-