StripperVentingBuilder Class¶
-
class
NXOpen.Tooling.
StripperVentingBuilder
¶ Bases:
NXOpen.Builder
Stripper Venting Builder of PDW and EDW.
A Body is returned by this builder. To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateStripperVentingBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Length | Returns the length of venting hole |
Radius | Returns the blend radius of venting hole |
SelectEdge | Returns the select edge for cutting venting hole |
Tag | Returns the Tag for this object. |
Width | Returns the width of venting hole |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Length¶
-
StripperVentingBuilder.
Length
¶ Returns the length of venting hole
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Radius¶
-
StripperVentingBuilder.
Radius
¶ Returns the blend radius of venting hole
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
SelectEdge¶
-
StripperVentingBuilder.
SelectEdge
¶ Returns the select edge for cutting venting hole
-------------------------------------
Getter Method
Signature
SelectEdge()
Returns: Return type: NXOpen.SelectEdgeList
New in version NX10.0.0.
License requirements: None.
Width¶
-
StripperVentingBuilder.
Width
¶ Returns the width of venting hole
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
StripperVentingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.