StripLayoutBuilderToStationType Enumeration¶
NXOpen.Tooling.StripLayoutBuilder.ToStationType is an alias for NXOpen.Tooling.StripLayoutBuilderToStationType
-
class
NXOpen.Tooling.
StripLayoutBuilderToStationType
¶ Bases:
object
Specifies the option of To Station for layout
Enum Members
Enum Member Enum Member Description One the end layout station is 1Two the end layout station is 2Three the end layout station is 3-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-