StockSizeBuilder Class¶
-
class
NXOpen.Tooling.
StockSizeBuilder
¶ Bases:
NXOpen.Builder
Represents a Tooling::StockSizeBuilder builder.
To create a new instance of this class, use
NXOpen.Tooling.StockSizeCollection.CreateStocksizeBuilder
Default values.
Property Value Clearance.Value 3.0 (millimeters part), 0.125 (inches part) IsClearanceAutoSet 0 ReferenceCsysType Wcs SizePrecision 3 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AxisVector | Returns or sets the cylinder axis vector to calculate cylinder stock szie |
BlankPrecisionValue | Returns or sets the blank size precision string. |
BlankSize | Returns or sets the blank size string, it is seperated by X . |
Clearance | Returns the clearance of the stocksize. |
ConnectionString | Returns or sets the connection string |
CylinderType | Returns or sets the cylinder type to generate a cylinder for the stock size. |
IsClearanceAutoSet | Returns or sets the is clearance auto set |
OffsetNegativeX | Returns or sets the clearance value for the blank in -X direction. |
OffsetNegativeY | Returns or sets the clearance value for the blank in -Y direction. |
OffsetNegativeZ | Returns or sets the clearance value for the blank in -Z direction. |
OffsetPositiveX | Returns or sets the clearance value for the blank in +X direction. |
OffsetPositiveY | Returns or sets the clearance value for the blank in +Y direction. |
OffsetPositiveZ | Returns or sets the clearance value for the blank in +Z direction. |
RadialOffset | Returns or sets the clearance value for the cylinder blank in radial direction. |
RefCsys | Returns or sets the reference csys to calculate stocksize. |
RefCsysSelection | Returns the reference csys to calculate stocksize. |
ReferenceCsysType | Returns or sets the reference csys type |
SelectBody | Returns the selected body to calculate a bounding box for stock size. |
SizePrecision | Returns or sets the size precision of the stock. |
StockType | Returns or sets the stock shape to be generated, it can be a box or cylinder. |
StringStock | Returns or sets the stock size string, it is seperated by X . |
Tag | Returns the Tag for this object. |
Type | Returns or sets the stock shape to be generated, it can be a block or cylinder. |
Methods¶
Method | Description |
---|---|
CalculateBoxSize | Calculate box size and get directions, edge length, lower point position. |
Commit | Commits any edits that have been applied to the builder. |
CreateRefCsys | Creates the reference csys for stock size. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditStockSizeAttr | Add or edit stock size attributes. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ModifyRefCsys | Modifies the reference csys for stock size. |
SetFitFaceStatus | Find out those extreme planar faces, and set fitting face status in all directions. |
SetManipulatorOrientation | Set the orientation of the current bounded box. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateBlankSizeString | Update blank size. |
UpdateStockSizeString | Update stock size. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StockSizeBuilderCylinder Enumeration | Represents the base circle type of cylinder. |
StockSizeBuilderRefCsysType Enumeration | Represents the reference CSYS type. |
StockSizeBuilderShape Enumeration | Represents the shape of stock size. |
StockSizeBuilderTypes Enumeration | Represents the shape of stock size. |
Property Detail¶
AxisVector¶
-
StockSizeBuilder.
AxisVector
¶ Returns or sets the cylinder axis vector to calculate cylinder stock szie
-------------------------------------
Getter Method
Signature
AxisVector()
Returns: Return type: NXOpen.Direction
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AxisVector(cylinderVector)
Parameters: cylinderVector ( NXOpen.Direction
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BlankPrecisionValue¶
-
StockSizeBuilder.
BlankPrecisionValue
¶ Returns or sets the blank size precision string.
-------------------------------------
Getter Method
Signature
BlankPrecisionValue()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankPrecisionValue(blankPrecisionValue)
Parameters: blankPrecisionValue (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
BlankSize¶
-
StockSizeBuilder.
BlankSize
¶ Returns or sets the blank size string, it is seperated by ” X ”.
-------------------------------------
Getter Method
Signature
BlankSize()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BlankSize(blankSize)
Parameters: blankSize (str) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Clearance¶
-
StockSizeBuilder.
Clearance
¶ Returns the clearance of the stocksize.
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
ConnectionString¶
-
StockSizeBuilder.
ConnectionString
¶ Returns or sets the connection string
-------------------------------------
Getter Method
Signature
ConnectionString()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConnectionString(connectionString)
Parameters: connectionString (str) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CylinderType¶
-
StockSizeBuilder.
CylinderType
¶ Returns or sets the cylinder type to generate a cylinder for the stock size.
-------------------------------------
Getter Method
Signature
CylinderType()
Returns: Return type: NXOpen.Tooling.StockSizeBuilderCylinder
New in version NX6.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
CylinderType(enumCylinderType)
Parameters: enumCylinderType ( NXOpen.Tooling.StockSizeBuilderCylinder
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
IsClearanceAutoSet¶
-
StockSizeBuilder.
IsClearanceAutoSet
¶ Returns or sets the is clearance auto set
-------------------------------------
Getter Method
Signature
IsClearanceAutoSet()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsClearanceAutoSet(isClearanceAutoSet)
Parameters: isClearanceAutoSet (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeX¶
-
StockSizeBuilder.
OffsetNegativeX
¶ Returns or sets the clearance value for the blank in -X direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeX()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetNegativeX(offsetNegativeX)
Parameters: offsetNegativeX (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeY¶
-
StockSizeBuilder.
OffsetNegativeY
¶ Returns or sets the clearance value for the blank in -Y direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeY()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetNegativeY(offsetNegativeY)
Parameters: offsetNegativeY (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetNegativeZ¶
-
StockSizeBuilder.
OffsetNegativeZ
¶ Returns or sets the clearance value for the blank in -Z direction.
-------------------------------------
Getter Method
Signature
OffsetNegativeZ()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetNegativeZ(offsetNegativeZ)
Parameters: offsetNegativeZ (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveX¶
-
StockSizeBuilder.
OffsetPositiveX
¶ Returns or sets the clearance value for the blank in +X direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveX()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetPositiveX(offsetPositiveX)
Parameters: offsetPositiveX (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveY¶
-
StockSizeBuilder.
OffsetPositiveY
¶ Returns or sets the clearance value for the blank in +Y direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveY()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetPositiveY(offsetPositiveY)
Parameters: offsetPositiveY (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
OffsetPositiveZ¶
-
StockSizeBuilder.
OffsetPositiveZ
¶ Returns or sets the clearance value for the blank in +Z direction.
-------------------------------------
Getter Method
Signature
OffsetPositiveZ()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetPositiveZ(offsetPositiveZ)
Parameters: offsetPositiveZ (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RadialOffset¶
-
StockSizeBuilder.
RadialOffset
¶ Returns or sets the clearance value for the cylinder blank in radial direction.
-------------------------------------
Getter Method
Signature
RadialOffset()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialOffset(radialOffset)
Parameters: radialOffset (float) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RefCsys¶
-
StockSizeBuilder.
RefCsys
¶ Returns or sets the reference csys to calculate stocksize.
-------------------------------------
Getter Method
Signature
RefCsys()
Returns: Return type: NXOpen.CoordinateSystem
New in version NX8.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
RefCsys(refCsys)
Parameters: refCsys ( NXOpen.CoordinateSystem
) –New in version NX8.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
RefCsysSelection¶
-
StockSizeBuilder.
RefCsysSelection
¶ Returns the reference csys to calculate stocksize.
-------------------------------------
Getter Method
Signature
RefCsysSelection()
Returns: Return type: NXOpen.SelectCoordinateSystem
New in version NX10.0.0.
License requirements: None.
ReferenceCsysType¶
-
StockSizeBuilder.
ReferenceCsysType
¶ Returns or sets the reference csys type
-------------------------------------
Getter Method
Signature
ReferenceCsysType()
Returns: Return type: NXOpen.Tooling.StockSizeBuilderRefCsysType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceCsysType(referenceCsysType)
Parameters: referenceCsysType ( NXOpen.Tooling.StockSizeBuilderRefCsysType
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectBody¶
-
StockSizeBuilder.
SelectBody
¶ Returns the selected body to calculate a bounding box for stock size.
-------------------------------------
Getter Method
Signature
SelectBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SizePrecision¶
-
StockSizeBuilder.
SizePrecision
¶ Returns or sets the size precision of the stock.
-------------------------------------
Getter Method
Signature
SizePrecision()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SizePrecision(integerPrecision)
Parameters: integerPrecision (int) – New in version NX6.0.0.
License requirements: None.
StockType¶
-
StockSizeBuilder.
StockType
¶ Returns or sets the stock shape to be generated, it can be a box or cylinder.
-------------------------------------
Getter Method
Signature
StockType()
Returns: Return type: NXOpen.Tooling.StockSizeBuilderShape
New in version NX6.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
-------------------------------------
Setter Method
Signature
StockType(enumStockType)
Parameters: enumStockType ( NXOpen.Tooling.StockSizeBuilderShape
) –New in version NX6.0.0.
Deprecated since version NX10.0.0: This functionality is no longer supported.
License requirements: None.
StringStock¶
-
StockSizeBuilder.
StringStock
¶ Returns or sets the stock size string, it is seperated by ” X ”.
-------------------------------------
Getter Method
Signature
StringStock()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StringStock(stringStock)
Parameters: stringStock (str) – New in version NX6.0.0.
License requirements: None.
Type¶
-
StockSizeBuilder.
Type
¶ Returns or sets the stock shape to be generated, it can be a block or cylinder.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.StockSizeBuilderTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.StockSizeBuilderTypes
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CalculateBoxSize¶
-
StockSizeBuilder.
CalculateBoxSize
¶ Calculate box size and get directions, edge length, lower point position.
Signature
CalculateBoxSize()
Returns: a tuple Return type: A tuple consisting of (minPoint, edgeLength, cysMatrix). minPoint is a NXOpen.Point3d
. edgeLength is a list of float. cysMatrix is aNXOpen.Matrix3x3
.New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
CreateRefCsys¶
-
StockSizeBuilder.
CreateRefCsys
¶ Creates the reference csys for stock size.
Signature
CreateRefCsys(inputOrigin, inputMatrix)
Parameters: - inputOrigin (
NXOpen.Point3d
) – - inputMatrix (
NXOpen.Matrix3x3
) –
New in version NX8.0.0.
License requirements: None.
- inputOrigin (
EditStockSizeAttr¶
-
StockSizeBuilder.
EditStockSizeAttr
¶ Add or edit stock size attributes.
Signature
EditStockSizeAttr(workPart)
Parameters: workPart ( NXOpen.NXObject
) –New in version NX8.0.0.
License requirements: None.
ModifyRefCsys¶
-
StockSizeBuilder.
ModifyRefCsys
¶ Modifies the reference csys for stock size.
Signature
ModifyRefCsys(inputOrigin, inputMatrix)
Parameters: - inputOrigin (
NXOpen.Point3d
) – - inputMatrix (
NXOpen.Matrix3x3
) –
New in version NX8.0.0.
License requirements: None.
- inputOrigin (
SetFitFaceStatus¶
-
StockSizeBuilder.
SetFitFaceStatus
¶ Find out those extreme planar faces, and set fitting face status in all directions.
Signature
SetFitFaceStatus(fitFace)
Parameters: fitFace (bool) – New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SetManipulatorOrientation¶
-
StockSizeBuilder.
SetManipulatorOrientation
¶ Set the orientation of the current bounded box.
Signature
SetManipulatorOrientation(cysMatrix)
Parameters: cysMatrix ( NXOpen.Matrix3x3
) –New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
UpdateBlankSizeString¶
-
StockSizeBuilder.
UpdateBlankSizeString
¶ Update blank size.
Signature
UpdateBlankSizeString()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
UpdateStockSizeString¶
-
StockSizeBuilder.
UpdateStockSizeString
¶ Update stock size.
Signature
UpdateStockSizeString()
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
StockSizeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.