SpreadsheetDataParameterStatus Enumeration¶
NXOpen.Tooling.SpreadsheetDataParameter.Status is an alias for NXOpen.Tooling.SpreadsheetDataParameterStatus
-
class
NXOpen.Tooling.
SpreadsheetDataParameterStatus
¶ Bases:
object
Represents the different spreadsheet parameter status
Enum Members
Enum Member Enum Member Description Lock User can’t change the value in UISystemKey This is system key parameterUserKey Key parameter analyzed from spreadsheet searchHideStatus Not shown in UIScaleItem This is a scale itemReadOnly This parameter is read onlyModified The parameter value is changedForceColor If the parameter uses user value, normally it shows in UI in a different color. If this status is set, the parameter value will be shown in the same color.HiddenValue The parameter has value, but it should be hidden to userOptionValue The parameter has multiple value, but not treated as key parameter-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-