ShimBuilder Class¶
-
class
NXOpen.Tooling.
ShimBuilder
¶ Bases:
NXOpen.Builder
Shim Builder of PDW and EDW.
A Body is returned by this builder. To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateShimBuilder
Default values.
Property Value ParentNode NoParent RenameToggle 0 New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Height | Returns the height of shim body |
InsertToDelete | Returns the shim component that needs to be deleted |
InsertToEdit | Returns the shim component that needs to be edit |
OffsetOuterDistance | Returns the offset distance of outer loop |
OuterRoughOffset | Returns or sets the outer rough offset |
ParentNode | Returns or sets the parent node which shim part will be insert to |
ParentPartName | Returns or sets the parent part name of shim part |
RenameToggle | Returns or sets the toggle to indicate whether to rename shim part |
ShimFace | Returns the face for doing shim body |
SlugholeProfile | Returns the list containing the inner profiles which need to offset. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
WizardType | Returns or sets the wizard type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateInnerProfileSetBuilder | Create a inner profile set builder object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ShimBuilderParentOption Enumeration | Specify the parent node. |
ShimBuilderTypes Enumeration | Specify the shim operation type. |
Property Detail¶
Height¶
-
ShimBuilder.
Height
¶ Returns the height of shim body
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
InsertToDelete¶
-
ShimBuilder.
InsertToDelete
¶ Returns the shim component that needs to be deleted
-------------------------------------
Getter Method
Signature
InsertToDelete()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX10.0.0.
License requirements: None.
InsertToEdit¶
-
ShimBuilder.
InsertToEdit
¶ Returns the shim component that needs to be edit
-------------------------------------
Getter Method
Signature
InsertToEdit()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX10.0.0.
License requirements: None.
OffsetOuterDistance¶
-
ShimBuilder.
OffsetOuterDistance
¶ Returns the offset distance of outer loop
-------------------------------------
Getter Method
Signature
OffsetOuterDistance()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
OuterRoughOffset¶
-
ShimBuilder.
OuterRoughOffset
¶ Returns or sets the outer rough offset
-------------------------------------
Getter Method
Signature
OuterRoughOffset()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OuterRoughOffset(outerRoughOffset)
Parameters: outerRoughOffset (bool) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ParentNode¶
-
ShimBuilder.
ParentNode
¶ Returns or sets the parent node which shim part will be insert to
-------------------------------------
Getter Method
Signature
ParentNode()
Returns: Return type: NXOpen.Tooling.ShimBuilderParentOption
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentNode(parentNode)
Parameters: parentNode ( NXOpen.Tooling.ShimBuilderParentOption
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ParentPartName¶
-
ShimBuilder.
ParentPartName
¶ Returns or sets the parent part name of shim part
-------------------------------------
Getter Method
Signature
ParentPartName()
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParentPartName(parentPartName)
Parameters: parentPartName (str) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
RenameToggle¶
-
ShimBuilder.
RenameToggle
¶ Returns or sets the toggle to indicate whether to rename shim part
-------------------------------------
Getter Method
Signature
RenameToggle()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenameToggle(renameToggle)
Parameters: renameToggle (bool) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
ShimFace¶
-
ShimBuilder.
ShimFace
¶ Returns the face for doing shim body
-------------------------------------
Getter Method
Signature
ShimFace()
Returns: Return type: NXOpen.SelectFaceList
New in version NX10.0.0.
License requirements: None.
SlugholeProfile¶
-
ShimBuilder.
SlugholeProfile
¶ Returns the list containing the inner profiles which need to offset.
-------------------------------------
Getter Method
Signature
SlugholeProfile()
Returns: Return type: NXOpen.Tooling.ShimInnerProfileSetBuilderList
New in version NX10.0.0.
License requirements: None.
Type¶
-
ShimBuilder.
Type
¶ Returns or sets the type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.ShimBuilderTypes
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.ShimBuilderTypes
) –New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
WizardType¶
-
ShimBuilder.
WizardType
¶ Returns or sets the wizard type
-------------------------------------
Getter Method
Signature
WizardType()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WizardType(wizardType)
Parameters: wizardType (int) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CreateInnerProfileSetBuilder¶
-
ShimBuilder.
CreateInnerProfileSetBuilder
¶ Create a inner profile set builder object.
Signature
CreateInnerProfileSetBuilder()
Returns: Return type: NXOpen.Tooling.ShimInnerProfileSetBuilder
New in version NX10.0.0.
License requirements: None.
Validate¶
-
ShimBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.