SectionLineCreationBuilder Class¶
-
class
NXOpen.Tooling.
SectionLineCreationBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.SectionLineCreationBuilder
which is used to create or edit the section line creation.To create a new instance of this class, use
NXOpen.Tooling.ToolingDrawingCollection.CreateSectionLineCreationBuilder
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
SelectPoint | Returns or sets the pnt select point |
Tag | Returns the Tag for this object. |
VectorDefineDirection | Returns or sets the vector direction |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateTemporaryLine | Create temporary line @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PointSubFunction | Define the cut segment position |
RemoveAll | Remove all cut segments |
RemoveLast | Remove the last cut segment |
ReverseVector | Reverse vector direction |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectPoint¶
-
SectionLineCreationBuilder.
SelectPoint
¶ Returns or sets the pnt select point
-------------------------------------
Getter Method
Signature
SelectPoint()
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectPoint(pntSelectPoint)
Parameters: pntSelectPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
VectorDefineDirection¶
-
SectionLineCreationBuilder.
VectorDefineDirection
¶ Returns or sets the vector direction
-------------------------------------
Getter Method
Signature
VectorDefineDirection()
Returns: Return type: NXOpen.Direction
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorDefineDirection(vectorDefineDirection)
Parameters: vectorDefineDirection ( NXOpen.Direction
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CreateTemporaryLine¶
-
SectionLineCreationBuilder.
CreateTemporaryLine
¶ Create temporary line
Signature
CreateTemporaryLine(pointData, direction)
Parameters: - pointData (
NXOpen.Point3d
) – - direction (
NXOpen.Vector3d
) –
Returns: Return type: New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- pointData (
PointSubFunction¶
-
SectionLineCreationBuilder.
PointSubFunction
¶ Define the cut segment position
Signature
PointSubFunction()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RemoveAll¶
-
SectionLineCreationBuilder.
RemoveAll
¶ Remove all cut segments
Signature
RemoveAll(curveList)
Parameters: curveList (list of NXOpen.Line
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
RemoveLast¶
-
SectionLineCreationBuilder.
RemoveLast
¶ Remove the last cut segment
Signature
RemoveLast(curveTag)
Parameters: curveTag ( NXOpen.Line
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
ReverseVector¶
-
SectionLineCreationBuilder.
ReverseVector
¶ Reverse vector direction
Signature
ReverseVector()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
SectionLineCreationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.