ScrapDesignBuilderScrapDefType Enumeration¶
NXOpen.Tooling.ScrapDesignBuilder.ScrapDefType is an alias for NXOpen.Tooling.ScrapDesignBuilderScrapDefType
-
class
NXOpen.Tooling.
ScrapDesignBuilderScrapDefType
¶ Bases:
object
Specifies the creation type of scraps
Enum Members
Enum Member Enum Member Description BlankBoundarySketch Boundary curves or sketch will be used to create scrapsHoleBoundary Hole boundary curves will be extracted automatically to create scrapsClosedCurves Close curves will be used to create scrapsBoundaryLines Boundary lines will be used to create an entire scrapExistedSheetBody Existed sheet body will be converted to scrapChangeType The type of scrap will be changed between Piercing and Piloting-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-