ScrapDesignBuilderScrapDefPosition Enumeration¶
NXOpen.Tooling.ScrapDesignBuilder.ScrapDefPosition is an alias for NXOpen.Tooling.ScrapDesignBuilderScrapDefPosition
-
class
NXOpen.Tooling.
ScrapDesignBuilderScrapDefPosition
¶ Bases:
object
Specifies the position method of scraps, projecting method is normally used
Enum Members
Enum Member Enum Member Description ProjectToStrip Scrap will be projected into the strip planeKeepOrigin Scrap will be created in the original plane-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-