RunnerBuilderGuideEndType Enumeration¶
NXOpen.Tooling.RunnerBuilder.GuideEndType is an alias for NXOpen.Tooling.RunnerBuilderGuideEndType
-
class
NXOpen.Tooling.
RunnerBuilderGuideEndType
¶ Bases:
object
Represents the runner guide end type.
Enum Members
Enum Member Enum Member Description Both Use both start and end points.StartOnly Use the start point only.EndOnly Use the end point only.None None of runner guide points for use.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-