QuickQuotationBuilderObjectTypes Enumeration¶
NXOpen.Tooling.QuickQuotationBuilder.ObjectTypes is an alias for NXOpen.Tooling.QuickQuotationBuilderObjectTypes
-
class
NXOpen.Tooling.
QuickQuotationBuilderObjectTypes
¶ Bases:
object
Specify the concept sheet body type.
Enum Members
Enum Member Enum Member Description Piercing sheet body type is piercing Bending sheet body type is piercing Forming sheet body is forming Burring sheet body is burring Cam sheet body is camunits. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-