PocketBuilder Class¶
-
class
NXOpen.Tooling.
PocketBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard pocket management builder
To create a new instance of this class, use
NXOpen.Tooling.PocketCollection.CreatePocketBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AssociationSetting | Returns or sets the association setting access functions |
CreateSolidSetting | Returns or sets the option for creating interference solids for HD3D. |
ModeSelection | Returns or sets the mode select types |
ReferenceSets | Returns or sets the types of reference sets |
SaveSetting | Returns or sets the option for saving pocket check result in part. |
SelectTarget | Returns the target part selection |
SelectTool | Returns the tool part selection |
SelectTypes | Returns or sets the types of tool to select |
ShowSetting | Returns or sets the show or hide value access functions |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CheckStatus | Checks the pocket status of standard parts |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindIntersection | Finds the intersected components to create pocket |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemovePocket | The function to remove pocket |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PocketBuilderModeType Enumeration | Represents the pocket operation method |
PocketBuilderRsetType Enumeration | Represents the pocket refset types |
PocketBuilderToolType Enumeration | Represents the select type of tool |
Property Detail¶
AssociationSetting¶
-
PocketBuilder.
AssociationSetting
¶ Returns or sets the association setting access functions
-------------------------------------
Getter Method
Signature
AssociationSetting()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AssociationSetting(associationSetting)
Parameters: associationSetting (bool) – New in version NX6.0.0.
License requirements: None.
CreateSolidSetting¶
-
PocketBuilder.
CreateSolidSetting
¶ Returns or sets the option for creating interference solids for HD3D.
-------------------------------------
Getter Method
Signature
CreateSolidSetting()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateSolidSetting(createSolidSetting)
Parameters: createSolidSetting (bool) – New in version NX8.0.0.
License requirements: None.
ModeSelection¶
-
PocketBuilder.
ModeSelection
¶ Returns or sets the mode select types
-------------------------------------
Getter Method
Signature
ModeSelection()
Returns: Return type: NXOpen.Tooling.PocketBuilderModeType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModeSelection(modeSelection)
Parameters: modeSelection ( NXOpen.Tooling.PocketBuilderModeType
) –New in version NX6.0.0.
License requirements: None.
ReferenceSets¶
-
PocketBuilder.
ReferenceSets
¶ Returns or sets the types of reference sets
-------------------------------------
Getter Method
Signature
ReferenceSets()
Returns: Return type: NXOpen.Tooling.PocketBuilderRsetType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceSets(referenceSets)
Parameters: referenceSets ( NXOpen.Tooling.PocketBuilderRsetType
) –New in version NX6.0.0.
License requirements: None.
SaveSetting¶
-
PocketBuilder.
SaveSetting
¶ Returns or sets the option for saving pocket check result in part.
-------------------------------------
Getter Method
Signature
SaveSetting()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveSetting(saveSetting)
Parameters: saveSetting (bool) – New in version NX8.0.0.
License requirements: None.
SelectTarget¶
-
PocketBuilder.
SelectTarget
¶ Returns the target part selection
-------------------------------------
Getter Method
Signature
SelectTarget()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SelectTool¶
-
PocketBuilder.
SelectTool
¶ Returns the tool part selection
-------------------------------------
Getter Method
Signature
SelectTool()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
SelectTypes¶
-
PocketBuilder.
SelectTypes
¶ Returns or sets the types of tool to select
-------------------------------------
Getter Method
Signature
SelectTypes()
Returns: Return type: NXOpen.Tooling.PocketBuilderToolType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectTypes(selectTypes)
Parameters: selectTypes ( NXOpen.Tooling.PocketBuilderToolType
) –New in version NX6.0.0.
License requirements: None.
ShowSetting¶
-
PocketBuilder.
ShowSetting
¶ Returns or sets the show or hide value access functions
-------------------------------------
Getter Method
Signature
ShowSetting()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowSetting(showSetting)
Parameters: showSetting (bool) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
CheckStatus¶
-
PocketBuilder.
CheckStatus
¶ Checks the pocket status of standard parts
Signature
CheckStatus()
New in version NX10.0.0.
License requirements: None.
FindIntersection¶
-
PocketBuilder.
FindIntersection
¶ Finds the intersected components to create pocket
Signature
FindIntersection()
New in version NX10.0.0.
License requirements: None.
RemovePocket¶
-
PocketBuilder.
RemovePocket
¶ The function to remove pocket
Signature
RemovePocket()
New in version NX6.0.0.
License requirements: None.
Validate¶
-
PocketBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.