MoldProcessBuilder Class¶
-
class
NXOpen.Tooling.
MoldProcessBuilder
¶ Bases:
NXOpen.Builder
Represents a Tooling::MoldProcessBuilder builder
To create a new instance of this class, use
NXOpen.Tooling.MoldProcessCollection.CreateMoldProcessBuilder
Default values.
Property Value Rename 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CompSelect | Returns the component selected to be edited. |
ConceptObjects | Returns the concept objects selected to be edited. |
Rename | Returns or sets the rename toggle let users choose whether to run Part Name Management dialog |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CompSelect¶
-
MoldProcessBuilder.
CompSelect
¶ Returns the component selected to be edited.
The edition will start Standard Part Management dialog
-------------------------------------
Getter Method
Signature
CompSelect()
Returns: Return type: NXOpen.SelectPoint
New in version NX6.0.0.
License requirements: None.
ConceptObjects¶
-
MoldProcessBuilder.
ConceptObjects
¶ Returns the concept objects selected to be edited.
-------------------------------------
Getter Method
Signature
ConceptObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
Rename¶
-
MoldProcessBuilder.
Rename
¶ Returns or sets the rename toggle let users choose whether to run Part Name Management dialog
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MoldProcessBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.