MoldInsertBuilder Class¶
-
class
NXOpen.Tooling.
MoldInsertBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard mold insert management builder
To create a new instance of this class, use
NXOpen.Tooling.MoldInsertCollection.CreateMoldInsertBuilder
Default values.
Property Value MethodType UniteSingleWorkpieces Rename 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
MethodType | Returns or sets the method type |
Rename | Returns or sets the rename method |
SelectBody | Returns the select body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MoldInsertBuilderBooleanType Enumeration | design type: unite single workpieces, subtract overall workpieces |
Property Detail¶
MethodType¶
-
MoldInsertBuilder.
MethodType
¶ Returns or sets the method type
-------------------------------------
Getter Method
Signature
MethodType()
Returns: Return type: NXOpen.Tooling.MoldInsertBuilderBooleanType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MethodType(methodType)
Parameters: methodType ( NXOpen.Tooling.MoldInsertBuilderBooleanType
) –New in version NX6.0.0.
License requirements: None.
Rename¶
-
MoldInsertBuilder.
Rename
¶ Returns or sets the rename method
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX6.0.0.
License requirements: None.
SelectBody¶
-
MoldInsertBuilder.
SelectBody
¶ Returns the select body
-------------------------------------
Getter Method
Signature
SelectBody()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MoldInsertBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.