MoldCsysBuilder Class¶
-
class
NXOpen.Tooling.
MoldCsysBuilder
¶ Bases:
NXOpen.Builder
Mold Wizard MoldCsys project builder
To create a new instance of this class, use
NXOpen.Tooling.MoldCsysCollection.CreateMoldCsysBuilder
Default values.
Property Value Lockx 0 Locky 0 Lockz 1 Wcstype CurrentWcs New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Lockx | Returns or sets the product doesn’t move along X to the new position of WCS if lockx is true |
Locky | Returns or sets the product doesn’t move along Y to the new position of WCS if locky is true |
Lockz | Returns or sets the product doesn’t move along Z to the new position of WCS if lockz is true |
Prod | Returns the selected faces are used to create a bounding box whose center will be the new origin of WCS |
Tag | Returns the Tag for this object. |
Wcstype | Returns or sets the wcs type to decide the method to get csys position |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MoldCsysBuilderWcsposition Enumeration | Represents the method to computer the WCS positino |
Property Detail¶
Lockx¶
-
MoldCsysBuilder.
Lockx
¶ Returns or sets the product doesn’t move along X to the new position of WCS if lockx is true
-------------------------------------
Getter Method
Signature
Lockx()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Lockx(lockx)
Parameters: lockx (bool) – New in version NX6.0.0.
License requirements: None.
Locky¶
-
MoldCsysBuilder.
Locky
¶ Returns or sets the product doesn’t move along Y to the new position of WCS if locky is true
-------------------------------------
Getter Method
Signature
Locky()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Locky(locky)
Parameters: locky (bool) – New in version NX6.0.0.
License requirements: None.
Lockz¶
-
MoldCsysBuilder.
Lockz
¶ Returns or sets the product doesn’t move along Z to the new position of WCS if lockz is true
-------------------------------------
Getter Method
Signature
Lockz()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Lockz(lockz)
Parameters: lockz (bool) – New in version NX6.0.0.
License requirements: None.
Prod¶
-
MoldCsysBuilder.
Prod
¶ Returns the selected faces are used to create a bounding box whose center will be the new origin of WCS
-------------------------------------
Getter Method
Signature
Prod()
Returns: Return type: NXOpen.SelectFaceList
New in version NX6.0.0.
License requirements: None.
Wcstype¶
-
MoldCsysBuilder.
Wcstype
¶ Returns or sets the wcs type to decide the method to get csys position
-------------------------------------
Getter Method
Signature
Wcstype()
Returns: Return type: NXOpen.Tooling.MoldCsysBuilderWcsposition
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Wcstype(wcstype)
Parameters: wcstype ( NXOpen.Tooling.MoldCsysBuilderWcsposition
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MoldCsysBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.