MWMoldedPartValidationBuilderAssignToRegion Enumeration¶
NXOpen.Tooling.MWMoldedPartValidationBuilder.AssignToRegion is an alias for NXOpen.Tooling.MWMoldedPartValidationBuilderAssignToRegion
-
class
NXOpen.Tooling.
MWMoldedPartValidationBuilderAssignToRegion
¶ Bases:
object
Options for assigning faces to the Cavity or Core region
Enum Members
Enum Member Enum Member Description CavityRegion assign selected region faces to the Cavity regionCoreRegion assign selected region faces to the Core region-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-