LsdynaGeometryPreparationBuilderBlankPosition Enumeration¶
NXOpen.Tooling.LsdynaGeometryPreparationBuilder.BlankPosition is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderBlankPosition
-
class
NXOpen.Tooling.
LsdynaGeometryPreparationBuilderBlankPosition
¶ Bases:
object
the enum of blank position.
Enum Members
Enum Member Enum Member Description AboveBinder Blank sheet body is above binder.AboveBinderandPunch Blank sheet body is above binder and punch.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-