LayoutRepositionBuilderMethod Enumeration¶
NXOpen.Tooling.LayoutRepositionBuilder.Method is an alias for NXOpen.Tooling.LayoutRepositionBuilderMethod
-
class
NXOpen.Tooling.
LayoutRepositionBuilderMethod
¶ Bases:
object
Represents the type of layout transform.
Enum Members
Enum Member Enum Member Description Rotate Rotate methodTransform Transform methodPointToPoint Point to Point method-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-