IntermediateStageCollection Class¶
-
class
NXOpen.Tooling.
IntermediateStageCollection
¶ Bases:
object
Creates a
NXOpen.Tooling.IntermediateStageBuilder
To obtain an instance of this class, refer to
NXOpen.Tooling.ToolingManager
New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
CreateIntermediateStageBuilder | Creates create direct unfold builder @return |
FindObject | Finds the NXOpen.Tooling.IntermediateStageBuilder with the given identifier as recorded in a journal. |
Method Detail¶
CreateIntermediateStageBuilder¶
-
IntermediateStageCollection.
CreateIntermediateStageBuilder
¶ Creates create direct unfold builder
Signature
CreateIntermediateStageBuilder()
Returns: Return type: NXOpen.Tooling.IntermediateStageBuilder
New in version NX8.5.0.
License requirements: None.
FindObject¶
-
IntermediateStageCollection.
FindObject
¶ Finds the
NXOpen.Tooling.IntermediateStageBuilder
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: IntermediateStageBuilder found Return type: NXOpen.Tooling.IntermediateStageBuilder
New in version NX8.5.0.
License requirements: None.