InsertAuxiliaryBuilder Class¶
-
class
NXOpen.Tooling.
InsertAuxiliaryBuilder
¶ Bases:
NXOpen.Builder
PDW insert auxiliary builder to design various auxiliaries of insert group
To create a new instance of this class, use
NXOpen.Tooling.InsertAuxiliaryCollection.CreateInsertAuxiliaryBuilder
Default values.
Property Value BottomPlateClearance 0 CircDeleteAllComponents 0 CircularOperation Create ClearanceValue 1 DesignTool Copy FalseBodyHeight.Value 0 (millimeters part), 0 (inches part) HeelHeight 5 HeelLength 10 HeelRadian 1 HeelWidth 5 OffsetAngle 0 OffsetX 0 OffsetY 0 PunchPlateClearance 0 PunchShankParaC 1 PunchShankParaFL 45 PunchShankParaL1 6 PunchShankParaLength 8 PunchShankParaPL 40 PunchShankParaR 13 PunchShankParaWidth 8 RampShankHeight.Value 0 (millimeters part), 0 (inches part) RectDeleteAllComponents 0 RectangularOperation Create ShankShape Flange StripperPlateClearance 0 TotalAlongX 1 TotalAlongY 1 TotalNumber 1 UseBottomPlateClearance 0 UseClearance 1 UsePunchPlateClearance 0 UseStripperPlateClearance 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BottomPlateClearance | Returns or sets the bottom plate clearance. |
CircDeleteAllComponents | Returns or sets the option to delete all components in circular array. |
CircularInsert | Returns the insert to do circular array. |
CircularOperation | Returns or sets the circular array operation. |
CircularVector | Returns or sets the specified vector for defining circular array axis. |
ClearanceValue | Returns or sets the clearance value. |
ControlPoint | Returns or sets the control point for the copy operation. |
CopySelectInsert | Returns the insert to be copied. |
DesignTool | Returns or sets the design tool. |
DestinationPoint | Returns or sets the destination point for the copy operation. |
FaceForRamp | Returns the sweep face for editing ramp. |
FalseBodyHeight | Returns the false body height. |
HeelHeight | Returns or sets the heel height. |
HeelLength | Returns or sets the heel length. |
HeelRadian | Returns or sets the heel radius. |
HeelWidth | Returns or sets the heel width. |
InsertEdge | Returns the insert edge. |
InsertShankFace | Returns the insert shank face. |
InsertsToDelete | Returns the insert objects to be deleted. |
MountPunchEdge | Returns the punch edge to place the mount. |
MountPunchFace | Returns the punch face to place the mount. |
OffsetAngle | Returns or sets the offset angle of circular array. |
OffsetX | Returns or sets the offset value along X. |
OffsetY | Returns or sets the offset value along Y. |
PointForRamp | Returns or sets the tangent point for the sweep guide curve |
Punch | Returns the selected punch. |
PunchEdge | Returns the punch edge. |
PunchPlateClearance | Returns or sets the punch plate clearance. |
PunchShankFace | Returns the punch shank. |
PunchShankParaC | Returns or sets the punch shank parameter for clearance between true body and false body. |
PunchShankParaFL | Returns or sets the punch shank parameter false body height. |
PunchShankParaL1 | Returns or sets the punch shank parameter for true body and false body length. |
PunchShankParaLength | Returns or sets the punch shank parameter length. |
PunchShankParaPL | Returns or sets the punch shank parameter for true body height. |
PunchShankParaR | Returns or sets the punch shank parameter for true body radius. |
PunchShankParaWidth | Returns or sets the punch shank parameter width. |
RadiusForRamp | Returns the the sweep guide curve radius. |
RampShankHeight | Returns the ramp shank height. |
RectDeleteAllComponents | Returns or sets the option to delete all components in rectangular array. |
RectangularInsert | Returns the insert to do rectangular array . |
RectangularOperation | Returns or sets the rectangular array operation. |
RectangularXVector | Returns or sets the X vector for rectangular array. |
RectangularYVector | Returns or sets the Y vector for rectangular array. |
SelectShankProfile | Returns the selected shank profile. |
ShankShape | Returns or sets the shank shape. |
ShanksToDelete | Returns the faces of those to be deleted shanks. |
StripperPlateClearance | Returns or sets the stripper plate clearance. |
Tag | Returns the Tag for this object. |
TotalAlongX | Returns or sets the total number of insert along X. |
TotalAlongY | Returns or sets the total number of insert along Y. |
TotalNumber | Returns or sets the total number of insert for circular array. |
Type | Returns or sets the insert auxiliary type. |
UseBottomPlateClearance | Returns or sets the option to use bottoming plate clearance. |
UseClearance | Returns or sets the option to use clearance. |
UsePunchPlateClearance | Returns or sets the option to use punch plate clearance. |
UseStripperPlateClearance | Returns or sets the option to stripper plate clearance. |
VectorForRamp | Returns or sets the vector to determintate the datum plane normal that the sweep guide curve in. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DesignMountHead | Design mount head for insert. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InsertAuxiliaryBuilderCircOperationTypes Enumeration | Specifies the options of circular array. |
InsertAuxiliaryBuilderDesignToolOption Enumeration | Specifies the design tool option. |
InsertAuxiliaryBuilderRectOperationOption Enumeration | Specifies the rectangular array option. |
InsertAuxiliaryBuilderShankShapeTypes Enumeration | Specifies the shank shape. |
InsertAuxiliaryBuilderTypes Enumeration | Specifies the insert auxiliary type. |
Property Detail¶
BottomPlateClearance¶
-
InsertAuxiliaryBuilder.
BottomPlateClearance
¶ Returns or sets the bottom plate clearance.
-------------------------------------
Getter Method
Signature
BottomPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BottomPlateClearance(bottomPlateClr)
Parameters: bottomPlateClr (float) – New in version NX7.5.0.
License requirements: None.
CircDeleteAllComponents¶
-
InsertAuxiliaryBuilder.
CircDeleteAllComponents
¶ Returns or sets the option to delete all components in circular array.
-------------------------------------
Getter Method
Signature
CircDeleteAllComponents()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircDeleteAllComponents(circDeleteAllComponents)
Parameters: circDeleteAllComponents (bool) – New in version NX7.5.0.
License requirements: None.
CircularInsert¶
-
InsertAuxiliaryBuilder.
CircularInsert
¶ Returns the insert to do circular array.
-------------------------------------
Getter Method
Signature
CircularInsert()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
CircularOperation¶
-
InsertAuxiliaryBuilder.
CircularOperation
¶ Returns or sets the circular array operation.
-------------------------------------
Getter Method
Signature
CircularOperation()
Returns: Return type: NXOpen.Tooling.InsertAuxiliaryBuilderCircOperationTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularOperation(circOperationType)
Parameters: circOperationType ( NXOpen.Tooling.InsertAuxiliaryBuilderCircOperationTypes
) –New in version NX7.5.0.
License requirements: None.
CircularVector¶
-
InsertAuxiliaryBuilder.
CircularVector
¶ Returns or sets the specified vector for defining circular array axis.
-------------------------------------
Getter Method
Signature
CircularVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CircularVector(circSpecifyVector)
Parameters: circSpecifyVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
ClearanceValue¶
-
InsertAuxiliaryBuilder.
ClearanceValue
¶ Returns or sets the clearance value.
-------------------------------------
Getter Method
Signature
ClearanceValue()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceValue(clearanceValue)
Parameters: clearanceValue (float) – New in version NX7.5.0.
License requirements: None.
ControlPoint¶
-
InsertAuxiliaryBuilder.
ControlPoint
¶ Returns or sets the control point for the copy operation.
-------------------------------------
Getter Method
Signature
ControlPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ControlPoint(specifyControlPoint)
Parameters: specifyControlPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: None.
CopySelectInsert¶
-
InsertAuxiliaryBuilder.
CopySelectInsert
¶ Returns the insert to be copied.
-------------------------------------
Getter Method
Signature
CopySelectInsert()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
DesignTool¶
-
InsertAuxiliaryBuilder.
DesignTool
¶ Returns or sets the design tool.
-------------------------------------
Getter Method
Signature
DesignTool()
Returns: Return type: NXOpen.Tooling.InsertAuxiliaryBuilderDesignToolOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignTool(designTool)
Parameters: designTool ( NXOpen.Tooling.InsertAuxiliaryBuilderDesignToolOption
) –New in version NX7.5.0.
License requirements: None.
DestinationPoint¶
-
InsertAuxiliaryBuilder.
DestinationPoint
¶ Returns or sets the destination point for the copy operation.
-------------------------------------
Getter Method
Signature
DestinationPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationPoint(specifyDestinationPoint)
Parameters: specifyDestinationPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: None.
FaceForRamp¶
-
InsertAuxiliaryBuilder.
FaceForRamp
¶ Returns the sweep face for editing ramp.
-------------------------------------
Getter Method
Signature
FaceForRamp()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
FalseBodyHeight¶
-
InsertAuxiliaryBuilder.
FalseBodyHeight
¶ Returns the false body height.
-------------------------------------
Getter Method
Signature
FalseBodyHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
HeelHeight¶
-
InsertAuxiliaryBuilder.
HeelHeight
¶ Returns or sets the heel height.
-------------------------------------
Getter Method
Signature
HeelHeight()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelHeight(heelHeight)
Parameters: heelHeight (float) – New in version NX7.5.0.
License requirements: None.
HeelLength¶
-
InsertAuxiliaryBuilder.
HeelLength
¶ Returns or sets the heel length.
-------------------------------------
Getter Method
Signature
HeelLength()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelLength(heelLength)
Parameters: heelLength (float) – New in version NX7.5.0.
License requirements: None.
HeelRadian¶
-
InsertAuxiliaryBuilder.
HeelRadian
¶ Returns or sets the heel radius.
-------------------------------------
Getter Method
Signature
HeelRadian()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelRadian(heelRadian)
Parameters: heelRadian (float) – New in version NX7.5.0.
License requirements: None.
HeelWidth¶
-
InsertAuxiliaryBuilder.
HeelWidth
¶ Returns or sets the heel width.
-------------------------------------
Getter Method
Signature
HeelWidth()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HeelWidth(heelWidth)
Parameters: heelWidth (float) – New in version NX7.5.0.
License requirements: None.
InsertEdge¶
-
InsertAuxiliaryBuilder.
InsertEdge
¶ Returns the insert edge.
-------------------------------------
Getter Method
Signature
InsertEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX7.5.0.
License requirements: None.
InsertShankFace¶
-
InsertAuxiliaryBuilder.
InsertShankFace
¶ Returns the insert shank face.
-------------------------------------
Getter Method
Signature
InsertShankFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
InsertsToDelete¶
-
InsertAuxiliaryBuilder.
InsertsToDelete
¶ Returns the insert objects to be deleted.
-------------------------------------
Getter Method
Signature
InsertsToDelete()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
MountPunchEdge¶
-
InsertAuxiliaryBuilder.
MountPunchEdge
¶ Returns the punch edge to place the mount.
-------------------------------------
Getter Method
Signature
MountPunchEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX7.5.0.
License requirements: None.
MountPunchFace¶
-
InsertAuxiliaryBuilder.
MountPunchFace
¶ Returns the punch face to place the mount.
-------------------------------------
Getter Method
Signature
MountPunchFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
OffsetAngle¶
-
InsertAuxiliaryBuilder.
OffsetAngle
¶ Returns or sets the offset angle of circular array.
-------------------------------------
Getter Method
Signature
OffsetAngle()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetAngle(offsetAngle)
Parameters: offsetAngle (float) – New in version NX7.5.0.
License requirements: None.
OffsetX¶
-
InsertAuxiliaryBuilder.
OffsetX
¶ Returns or sets the offset value along X.
-------------------------------------
Getter Method
Signature
OffsetX()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetX(offsetX)
Parameters: offsetX (float) – New in version NX7.5.0.
License requirements: None.
OffsetY¶
-
InsertAuxiliaryBuilder.
OffsetY
¶ Returns or sets the offset value along Y.
-------------------------------------
Getter Method
Signature
OffsetY()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetY(offsetY)
Parameters: offsetY (float) – New in version NX7.5.0.
License requirements: None.
PointForRamp¶
-
InsertAuxiliaryBuilder.
PointForRamp
¶ Returns or sets the tangent point for the sweep guide curve
-------------------------------------
Getter Method
Signature
PointForRamp()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointForRamp(pointForRamp)
Parameters: pointForRamp ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: None.
Punch¶
-
InsertAuxiliaryBuilder.
Punch
¶ Returns the selected punch.
-------------------------------------
Getter Method
Signature
Punch()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
PunchEdge¶
-
InsertAuxiliaryBuilder.
PunchEdge
¶ Returns the punch edge.
-------------------------------------
Getter Method
Signature
PunchEdge()
Returns: Return type: NXOpen.SelectEdge
New in version NX7.5.0.
License requirements: None.
PunchPlateClearance¶
-
InsertAuxiliaryBuilder.
PunchPlateClearance
¶ Returns or sets the punch plate clearance.
-------------------------------------
Getter Method
Signature
PunchPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchPlateClearance(punchPlateClr)
Parameters: punchPlateClr (float) – New in version NX7.5.0.
License requirements: None.
PunchShankFace¶
-
InsertAuxiliaryBuilder.
PunchShankFace
¶ Returns the punch shank.
-------------------------------------
Getter Method
Signature
PunchShankFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
PunchShankParaC¶
-
InsertAuxiliaryBuilder.
PunchShankParaC
¶ Returns or sets the punch shank parameter for clearance between true body and false body.
-------------------------------------
Getter Method
Signature
PunchShankParaC()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaC(punchShankParaC)
Parameters: punchShankParaC (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaFL¶
-
InsertAuxiliaryBuilder.
PunchShankParaFL
¶ Returns or sets the punch shank parameter false body height.
-------------------------------------
Getter Method
Signature
PunchShankParaFL()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaFL(punchShankParaFL)
Parameters: punchShankParaFL (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaL1¶
-
InsertAuxiliaryBuilder.
PunchShankParaL1
¶ Returns or sets the punch shank parameter for true body and false body length.
-------------------------------------
Getter Method
Signature
PunchShankParaL1()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaL1(punchShankParaL1)
Parameters: punchShankParaL1 (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaLength¶
-
InsertAuxiliaryBuilder.
PunchShankParaLength
¶ Returns or sets the punch shank parameter length.
-------------------------------------
Getter Method
Signature
PunchShankParaLength()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaLength(punchShankParaL)
Parameters: punchShankParaL (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaPL¶
-
InsertAuxiliaryBuilder.
PunchShankParaPL
¶ Returns or sets the punch shank parameter for true body height.
-------------------------------------
Getter Method
Signature
PunchShankParaPL()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaPL(punchShankParaPL)
Parameters: punchShankParaPL (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaR¶
-
InsertAuxiliaryBuilder.
PunchShankParaR
¶ Returns or sets the punch shank parameter for true body radius.
-------------------------------------
Getter Method
Signature
PunchShankParaR()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaR(punchShankParaR)
Parameters: punchShankParaR (float) – New in version NX7.5.0.
License requirements: None.
PunchShankParaWidth¶
-
InsertAuxiliaryBuilder.
PunchShankParaWidth
¶ Returns or sets the punch shank parameter width.
-------------------------------------
Getter Method
Signature
PunchShankParaWidth()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PunchShankParaWidth(punchShankParaW)
Parameters: punchShankParaW (float) – New in version NX7.5.0.
License requirements: None.
RadiusForRamp¶
-
InsertAuxiliaryBuilder.
RadiusForRamp
¶ Returns the the sweep guide curve radius.
-------------------------------------
Getter Method
Signature
RadiusForRamp()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
RampShankHeight¶
-
InsertAuxiliaryBuilder.
RampShankHeight
¶ Returns the ramp shank height.
-------------------------------------
Getter Method
Signature
RampShankHeight()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
RectDeleteAllComponents¶
-
InsertAuxiliaryBuilder.
RectDeleteAllComponents
¶ Returns or sets the option to delete all components in rectangular array.
-------------------------------------
Getter Method
Signature
RectDeleteAllComponents()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectDeleteAllComponents(rectDeleteAllComponents)
Parameters: rectDeleteAllComponents (bool) – New in version NX7.5.0.
License requirements: None.
RectangularInsert¶
-
InsertAuxiliaryBuilder.
RectangularInsert
¶ Returns the insert to do rectangular array .
-------------------------------------
Getter Method
Signature
RectangularInsert()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
RectangularOperation¶
-
InsertAuxiliaryBuilder.
RectangularOperation
¶ Returns or sets the rectangular array operation.
-------------------------------------
Getter Method
Signature
RectangularOperation()
Returns: Return type: NXOpen.Tooling.InsertAuxiliaryBuilderRectOperationOption
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangularOperation(rectOperationType)
Parameters: rectOperationType ( NXOpen.Tooling.InsertAuxiliaryBuilderRectOperationOption
) –New in version NX7.5.0.
License requirements: None.
RectangularXVector¶
-
InsertAuxiliaryBuilder.
RectangularXVector
¶ Returns or sets the X vector for rectangular array.
-------------------------------------
Getter Method
Signature
RectangularXVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangularXVector(rectSpecifyVectorX)
Parameters: rectSpecifyVectorX ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
RectangularYVector¶
-
InsertAuxiliaryBuilder.
RectangularYVector
¶ Returns or sets the Y vector for rectangular array.
-------------------------------------
Getter Method
Signature
RectangularYVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RectangularYVector(rectSpecifyVectorY)
Parameters: rectSpecifyVectorY ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
SelectShankProfile¶
-
InsertAuxiliaryBuilder.
SelectShankProfile
¶ Returns the selected shank profile.
-------------------------------------
Getter Method
Signature
SelectShankProfile()
Returns: Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
ShankShape¶
-
InsertAuxiliaryBuilder.
ShankShape
¶ Returns or sets the shank shape.
-------------------------------------
Getter Method
Signature
ShankShape()
Returns: Return type: NXOpen.Tooling.InsertAuxiliaryBuilderShankShapeTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShankShape(shankShape)
Parameters: shankShape ( NXOpen.Tooling.InsertAuxiliaryBuilderShankShapeTypes
) –New in version NX7.5.0.
License requirements: None.
ShanksToDelete¶
-
InsertAuxiliaryBuilder.
ShanksToDelete
¶ Returns the faces of those to be deleted shanks.
-------------------------------------
Getter Method
Signature
ShanksToDelete()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
StripperPlateClearance¶
-
InsertAuxiliaryBuilder.
StripperPlateClearance
¶ Returns or sets the stripper plate clearance.
-------------------------------------
Getter Method
Signature
StripperPlateClearance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StripperPlateClearance(stripperPlateClr)
Parameters: stripperPlateClr (float) – New in version NX7.5.0.
License requirements: None.
TotalAlongX¶
-
InsertAuxiliaryBuilder.
TotalAlongX
¶ Returns or sets the total number of insert along X.
-------------------------------------
Getter Method
Signature
TotalAlongX()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TotalAlongX(totalNumberX)
Parameters: totalNumberX (int) – New in version NX7.5.0.
License requirements: None.
TotalAlongY¶
-
InsertAuxiliaryBuilder.
TotalAlongY
¶ Returns or sets the total number of insert along Y.
-------------------------------------
Getter Method
Signature
TotalAlongY()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TotalAlongY(totalNumberY)
Parameters: totalNumberY (int) – New in version NX7.5.0.
License requirements: None.
TotalNumber¶
-
InsertAuxiliaryBuilder.
TotalNumber
¶ Returns or sets the total number of insert for circular array.
-------------------------------------
Getter Method
Signature
TotalNumber()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TotalNumber(totalNumber)
Parameters: totalNumber (int) – New in version NX7.5.0.
License requirements: None.
Type¶
-
InsertAuxiliaryBuilder.
Type
¶ Returns or sets the insert auxiliary type.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.InsertAuxiliaryBuilderTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.InsertAuxiliaryBuilderTypes
) –New in version NX7.5.0.
License requirements: None.
UseBottomPlateClearance¶
-
InsertAuxiliaryBuilder.
UseBottomPlateClearance
¶ Returns or sets the option to use bottoming plate clearance.
-------------------------------------
Getter Method
Signature
UseBottomPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseBottomPlateClearance(useBPClearance)
Parameters: useBPClearance (bool) – New in version NX7.5.0.
License requirements: None.
UseClearance¶
-
InsertAuxiliaryBuilder.
UseClearance
¶ Returns or sets the option to use clearance.
-------------------------------------
Getter Method
Signature
UseClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseClearance(useClearance)
Parameters: useClearance (bool) – New in version NX7.5.0.
License requirements: None.
UsePunchPlateClearance¶
-
InsertAuxiliaryBuilder.
UsePunchPlateClearance
¶ Returns or sets the option to use punch plate clearance.
-------------------------------------
Getter Method
Signature
UsePunchPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UsePunchPlateClearance(usePPClearance)
Parameters: usePPClearance (bool) – New in version NX7.5.0.
License requirements: None.
UseStripperPlateClearance¶
-
InsertAuxiliaryBuilder.
UseStripperPlateClearance
¶ Returns or sets the option to stripper plate clearance.
-------------------------------------
Getter Method
Signature
UseStripperPlateClearance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseStripperPlateClearance(useSPClearance)
Parameters: useSPClearance (bool) – New in version NX7.5.0.
License requirements: None.
VectorForRamp¶
-
InsertAuxiliaryBuilder.
VectorForRamp
¶ Returns or sets the vector to determintate the datum plane normal that the sweep guide curve in.
-------------------------------------
Getter Method
Signature
VectorForRamp()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
VectorForRamp(vectorForRamp)
Parameters: vectorForRamp ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
DesignMountHead¶
-
InsertAuxiliaryBuilder.
DesignMountHead
¶ Design mount head for insert.
Signature
DesignMountHead()
New in version NX7.5.0.
License requirements: None.
Validate¶
-
InsertAuxiliaryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.