HoleManufacturingNoteBuilder Class¶
-
class
NXOpen.Tooling.
HoleManufacturingNoteBuilder
¶ Bases:
NXOpen.Builder
Tooling builder for HoleManufacturingNote
To create a new instance of this class, use
NXOpen.Tooling.HoleManufacturingNoteCollection.CreateHoleManufacturingNoteBuilder
Default values.
Property Value DefineByViewOrHolesEnum View HoleIndexSize 3.5 HoleIndexTypeEnum UserDefinedAndNumber HoleManufacturingNoteSize 3.5 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CreatedHoleManufacturingNote | Returns or sets the created hole manufacturing note |
DefineByViewOrHolesEnum | Returns or sets the selection type enumeration |
HoleIndexColor | Returns or sets the hole index character color |
HoleIndexSize | Returns or sets the hole index character size |
HoleIndexTypeEnum | Returns or sets the hole index type enumeration |
HoleManufacturingNoteColor | Returns or sets the manufaturing information character color |
HoleManufacturingNoteOrigin | Returns the manufacturing information origin |
HoleManufacturingNoteSize | Returns or sets the manufaturing information character size |
HoleManufacturingNoteStyle | Returns the hole manufacturing note style |
SelectHoles | Returns the selected holes |
SelectView | Returns the selected view |
Tag | Returns the Tag for this object. |
WizardType | Returns or sets the wizard type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateHoleIndexLabel | The method to create hole index @return The hole index label tag |
CreateHoleManufacturingNoteAsNote | The method to create manufaturing information as note @return The manufaturing information note tag |
CycleObjectsInView | The method to cycle objects in view @return Output object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ModifyStyle | The method to modify the style of the previewed note |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
HoleManufacturingNoteBuilderDefineByViewOrHoles Enumeration | the view selection or window selection type |
HoleManufacturingNoteBuilderHoleIndexType Enumeration | the hole index type |
Property Detail¶
CreatedHoleManufacturingNote¶
-
HoleManufacturingNoteBuilder.
CreatedHoleManufacturingNote
¶ Returns or sets the created hole manufacturing note
-------------------------------------
Getter Method
Signature
CreatedHoleManufacturingNote()
Returns: Return type: NXOpen.NXObject
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreatedHoleManufacturingNote(createdHoleManufacturingNote)
Parameters: createdHoleManufacturingNote ( NXOpen.NXObject
) –New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DefineByViewOrHolesEnum¶
-
HoleManufacturingNoteBuilder.
DefineByViewOrHolesEnum
¶ Returns or sets the selection type enumeration
-------------------------------------
Getter Method
Signature
DefineByViewOrHolesEnum()
Returns: Return type: NXOpen.Tooling.HoleManufacturingNoteBuilderDefineByViewOrHoles
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefineByViewOrHolesEnum(defineByViewOrHoles)
Parameters: defineByViewOrHoles ( NXOpen.Tooling.HoleManufacturingNoteBuilderDefineByViewOrHoles
) –New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleIndexColor¶
-
HoleManufacturingNoteBuilder.
HoleIndexColor
¶ Returns or sets the hole index character color
-------------------------------------
Getter Method
Signature
HoleIndexColor()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleIndexColor(holeIndexColor)
Parameters: holeIndexColor (Id) – New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleIndexSize¶
-
HoleManufacturingNoteBuilder.
HoleIndexSize
¶ Returns or sets the hole index character size
-------------------------------------
Getter Method
Signature
HoleIndexSize()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleIndexSize(holeIndexSize)
Parameters: holeIndexSize (float) – New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleIndexTypeEnum¶
-
HoleManufacturingNoteBuilder.
HoleIndexTypeEnum
¶ Returns or sets the hole index type enumeration
-------------------------------------
Getter Method
Signature
HoleIndexTypeEnum()
Returns: Return type: NXOpen.Tooling.HoleManufacturingNoteBuilderHoleIndexType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleIndexTypeEnum(holeIndexTypeEnum)
Parameters: holeIndexTypeEnum ( NXOpen.Tooling.HoleManufacturingNoteBuilderHoleIndexType
) –New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleManufacturingNoteColor¶
-
HoleManufacturingNoteBuilder.
HoleManufacturingNoteColor
¶ Returns or sets the manufaturing information character color
-------------------------------------
Getter Method
Signature
HoleManufacturingNoteColor()
Returns: Return type: Id New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleManufacturingNoteColor(holeManufacturingNoteColor)
Parameters: holeManufacturingNoteColor (Id) – New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleManufacturingNoteOrigin¶
-
HoleManufacturingNoteBuilder.
HoleManufacturingNoteOrigin
¶ Returns the manufacturing information origin
-------------------------------------
Getter Method
Signature
HoleManufacturingNoteOrigin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX9.0.0.
License requirements: None.
HoleManufacturingNoteSize¶
-
HoleManufacturingNoteBuilder.
HoleManufacturingNoteSize
¶ Returns or sets the manufaturing information character size
-------------------------------------
Getter Method
Signature
HoleManufacturingNoteSize()
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
HoleManufacturingNoteSize(holeManufacturingNoteSize)
Parameters: holeManufacturingNoteSize (float) – New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
HoleManufacturingNoteStyle¶
-
HoleManufacturingNoteBuilder.
HoleManufacturingNoteStyle
¶ Returns the hole manufacturing note style
-------------------------------------
Getter Method
Signature
HoleManufacturingNoteStyle()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX9.0.0.
License requirements: None.
SelectHoles¶
-
HoleManufacturingNoteBuilder.
SelectHoles
¶ Returns the selected holes
-------------------------------------
Getter Method
Signature
SelectHoles()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
SelectView¶
-
HoleManufacturingNoteBuilder.
SelectView
¶ Returns the selected view
-------------------------------------
Getter Method
Signature
SelectView()
Returns: Return type: NXOpen.SelectNXObject
New in version NX9.0.0.
License requirements: None.
WizardType¶
-
HoleManufacturingNoteBuilder.
WizardType
¶ Returns or sets the wizard type
-------------------------------------
Getter Method
Signature
WizardType()
Returns: Return type: int New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WizardType(wizardType)
Parameters: wizardType (int) – New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
CreateHoleIndexLabel¶
-
HoleManufacturingNoteBuilder.
CreateHoleIndexLabel
¶ The method to create hole index
Signature
CreateHoleIndexLabel(viewTag, holeTypeIndex, faceTag, holeDiameter, holePos, holetype, reverseFlag)
Parameters: - viewTag (
NXOpen.NXObject
) – The view to create hole index label - holeTypeIndex (str) – The hole hole index label string NOTE: The full Unicode character set is not supported for this parameter.
- faceTag (
NXOpen.NXObject
) – The hole face data - holeDiameter (float) – The hole diameter
- holePos (
NXOpen.Point3d
) – The hole position - holetype (str) – The hole type string NOTE: The full Unicode character set is not supported for this parameter.
- reverseFlag (bool) – The hole reversed flag
Returns: The hole index label tag
Return type: New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- viewTag (
CreateHoleManufacturingNoteAsNote¶
-
HoleManufacturingNoteBuilder.
CreateHoleManufacturingNoteAsNote
¶ The method to create manufaturing information as note
Signature
CreateHoleManufacturingNoteAsNote(viewTag, holeManufacturingNoteVector, point)
Parameters: - viewTag (
NXOpen.NXObject
) – The view to create hole index label - holeManufacturingNoteVector (list of str) – The hole index label string NOTE: The full Unicode character set is not supported for this parameter.
- point (
NXOpen.Point3d
) – The location point data
Returns: The manufaturing information note tag
Return type: New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- viewTag (
CycleObjectsInView¶
-
HoleManufacturingNoteBuilder.
CycleObjectsInView
¶ The method to cycle objects in view
Signature
CycleObjectsInView(viewTag, vseqNumber, isDrawing, inObject)
Parameters: - viewTag (
NXOpen.NXObject
) – The view to cycle - vseqNumber (int) – The View Sequence Number of the View must NOT be DSS_ALL_VIEWS or DSS_NO_VIEWS
- isDrawing (bool) – Is this view a drawing
- inObject (
NXOpen.NXObject
) – Input object
Returns: Output object
Return type: New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- viewTag (
ModifyStyle¶
-
HoleManufacturingNoteBuilder.
ModifyStyle
¶ The method to modify the style of the previewed note
Signature
ModifyStyle()
New in version NX9.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
HoleManufacturingNoteBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.