HemFixerBuilder Class¶
-
class
NXOpen.Tooling.
HemFixerBuilder
¶ Bases:
NXOpen.Builder
Hem Fixer Builder of PDW and EDW.
A Body is returned by this builder. To create a new instance of this class, use
NXOpen.Tooling.ProgressiveDieManager.CreateHemFixerBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BendFace | Returns the bend face that connects flange and base body |
BendRadius | Returns the bend radius that defines radius of inner bend face |
FlangeFace | Returns the flange faces that will be offset for creating gap between flange and base body |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BendFace¶
-
HemFixerBuilder.
BendFace
¶ Returns the bend face that connects flange and base body
-------------------------------------
Getter Method
Signature
BendFace()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
BendRadius¶
-
HemFixerBuilder.
BendRadius
¶ Returns the bend radius that defines radius of inner bend face
-------------------------------------
Getter Method
Signature
BendRadius()
Returns: Return type: NXOpen.Expression
New in version NX10.0.0.
License requirements: None.
FlangeFace¶
-
HemFixerBuilder.
FlangeFace
¶ Returns the flange faces that will be offset for creating gap between flange and base body
-------------------------------------
Getter Method
Signature
FlangeFace()
Returns: Return type: NXOpen.ScCollector
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
HemFixerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.