ForceCalculationBuilderCalculationTypes Enumeration¶
NXOpen.Tooling.ForceCalculationBuilder.CalculationTypes is an alias for NXOpen.Tooling.ForceCalculationBuilderCalculationTypes
-
class
NXOpen.Tooling.
ForceCalculationBuilderCalculationTypes
¶ Bases:
object
The calculation type.
Enum Members
Enum Member Enum Member Description Normal calculate force considering pre-stations effectsIsolated calculate force in isolation, without considering other processes-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-