FlowDisplayBuilder Class¶
-
class
NXOpen.Tooling.
FlowDisplayBuilder
¶ Bases:
NXOpen.Builder
Represents the builder which is used to create flow analysis.
To create a new instance of this class, use
NXOpen.Tooling.MoldDesignCollection.CreateFlowDisplayBuilder
Default values.
Property Value AirTrapOption 0 NumberIntervals 20 NumberSubMeshes 0 ResultsOption MeltFrontTime WeldLineOption 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
AirTrapOption | Returns or sets the air trap option to be set |
FolderBrowser | Returns or sets the folder in which flow analysis results can be found |
NumberIntervals | Returns or sets the interval number of the whole filling time. |
NumberSubMeshes | Returns or sets the number of sub-meshes to display |
ResultsOption | Returns or sets the analysis results option to display |
Tag | Returns the Tag for this object. |
WeldLineOption | Returns or sets the weld line option to be set |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayDynamicColorPlots | Display color plots in all steps. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FlowDisplayBuilderAnalysisResults Enumeration | The option of analysis results. |
Property Detail¶
AirTrapOption¶
-
FlowDisplayBuilder.
AirTrapOption
¶ Returns or sets the air trap option to be set
-------------------------------------
Getter Method
Signature
AirTrapOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AirTrapOption(airTrapOption)
Parameters: airTrapOption (bool) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
FolderBrowser¶
-
FlowDisplayBuilder.
FolderBrowser
¶ Returns or sets the folder in which flow analysis results can be found
-------------------------------------
Getter Method
Signature
FolderBrowser()
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FolderBrowser(foldername)
Parameters: foldername (str) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
NumberIntervals¶
-
FlowDisplayBuilder.
NumberIntervals
¶ Returns or sets the interval number of the whole filling time.
-------------------------------------
Getter Method
Signature
NumberIntervals()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberIntervals(numIntervals)
Parameters: numIntervals (int) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
NumberSubMeshes¶
-
FlowDisplayBuilder.
NumberSubMeshes
¶ Returns or sets the number of sub-meshes to display
-------------------------------------
Getter Method
Signature
NumberSubMeshes()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberSubMeshes(noSubMeshes)
Parameters: noSubMeshes (int) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
ResultsOption¶
-
FlowDisplayBuilder.
ResultsOption
¶ Returns or sets the analysis results option to display
-------------------------------------
Getter Method
Signature
ResultsOption()
Returns: Return type: NXOpen.Tooling.FlowDisplayBuilderAnalysisResults
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultsOption(resultsOption)
Parameters: resultsOption ( NXOpen.Tooling.FlowDisplayBuilderAnalysisResults
) –New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
WeldLineOption¶
-
FlowDisplayBuilder.
WeldLineOption
¶ Returns or sets the weld line option to be set
-------------------------------------
Getter Method
Signature
WeldLineOption()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldLineOption(weldLineOption)
Parameters: weldLineOption (bool) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
Method Detail¶
DisplayDynamicColorPlots¶
-
FlowDisplayBuilder.
DisplayDynamicColorPlots
¶ Display color plots in all steps.
Signature
DisplayDynamicColorPlots()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”)
Validate¶
-
FlowDisplayBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.