FastenerAssy Class¶
-
class
NXOpen.Tooling.
FastenerAssy
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.FastenerAssy
To create a new instance of this class, use
NXOpen.Tooling.FastenerAssyCollection.CreateBuilder
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
AddParentNewPart | Adds new part for the parent node |
AddRemovalHoleIndex | Add the removal hole index in the fastener setup data |
AddScrewArray | Adds stack array |
AddTopNode | Adds top node for the fastener assembly @return Output the instance of the parent node |
AdjustFastenerLength | Adjusts the fastener assembly length |
Commit | Commits any edits that have been applied to the builder. |
CreateArrayHole | Creates array hole data for the fastener assembly |
CreateFastenerConstraints | Creates fastener assembly constraint |
CreateReusableBuilder | Creates new reusable builder @return the new NXOpen.Tooling.AddReusablePart instance |
CreateReusablePocket | Creates reusable pocket |
CreateSameAssemblyData | Creates the same assembly data type |
DeleteArrayHole | Deletes array hole data for the fastener assembly |
DeleteReusablePocket | Deletes reusable pocket |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EraseAssemblyData | Erases the assembly data |
EraseFastenerAssembly | Erases fastener assembly |
EraseFastenerAssemblyData | Erases the fastener assembly data, including the hole data and assembly data in the fastener setup data |
EraseFastenerSetupData | Erases the data (hole and assembly data) in fastener assembly |
EraseStackArray | Erases stack array |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFastenerMode | Gets the fastener mode @return |
GetFastenerSelectionType | Gets the selection type for the hole in the fastener assembly @return The selection type to add the fastener assembly |
GetObject | Returns the object currently being edited by this builder. |
GetReusablePocketBuilder | Gets the reusable pocket builder @return The reusable component pocket builder |
InitPocketBuilder | Inits pocket builder |
ReadAssemblyConfigure | Reads fastener assembly configuration data from the hole data |
RemoveFastenerConstraints | Removes fastener assembly constraint |
RemoveSelectedHole | Removes the selected hole from the fastener setup data |
RenameParentNode | Renames the parent node |
SaveUdoData | Saves UDO data for fastener assembly |
SelectScrewSize | Selects the screw size |
SetAssemblyExtentLength | Sets the extent length for the fastener assembly data |
SetBlindHole | Sets the blind hole for the hole in the fastener assembly |
SetCreatePocket | Sets the flag to indicate whether to create pocket when adding the fastener |
SetDefaultPlanarFaces | Sets the default planar face for the hole in the fastener assembly |
SetFastenerExtentLength | Sets the extent length for the hole in the fastener assembly |
SetFastenerMode | Sets the fastener mode |
SetFastenerSelectionType | Sets the selection type for the hole in the fastener assembly |
SetHoleDefaultCylindricalFace | Sets the default cylindrical face for the hole in the fastener assembly |
SetHoleDiameter | Sets the diameter for the hole in the fastener assembly |
SetHoleDirection | Sets the direction for the hole in the fastener assembly |
SetHoleFaces | Sets the faces for the hole in the fastener assembly |
SetHoleHeight | Sets the height for the hole in the fastener assembly |
SetHoleOriginDiameter | Sets the origin diameter for the hole in the fastener assembly |
SetHoleOriginHeight | Sets the origin height for the hole in the fastener assembly |
SetHoleOriginPosition | Sets the origin position for the hole in the fastener assembly |
SetHolePosition | Sets the position for the hole in the fastener assembly |
SetHoleSideCylindricalFaces | Sets the side cylindrical faces for the hole in the fastener assembly |
SetInstanceFeatureFaces | Sets the instance feature face for the hole in the fastener assembly |
SetItemName | Adds item description for the part |
SetReusablePocketBuilder | Sets the reusable pocket builder |
SetReuseBuilder | Sets the reuse builder |
SetSidePlanarFaces | Sets the side planar faces for the hole in the fastener assembly |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SubstituteFastenerStack | Substitutes fastener stack |
UpdateDefaultStandard | Updates default standard hole data for the fastener assembly configuration |
UpdateFastenerLength | Updates the fastener length |
UpdateFastenerStacks | Updates fastener stacks |
UpdateHoleData | Updates the hole data |
UpdateHolePostion | Updates the hole positon for position method |
UpdateStackPosition | Updates the fastener assembly after changing stacks or changing stack properties |
UpdateTopBottomStacks | Updates fastener assembly according to the new extends |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FastenerAssyHoleOperation Enumeration | Represents the action on the hole menu of the fastener assembly. |
FastenerAssyModeMethod Enumeration | Represents adding and editing modes for the fastener assembly |
FastenerAssySelectionObjectMethod Enumeration | Represents selection object type |
FastenerAssySelectionTypeMethod Enumeration | Represents selection type for position and hole |
FastenerAssyStackTypeMethod Enumeration | Represents screw_array type |
Method Detail¶
AddParentNewPart¶
-
FastenerAssy.
AddParentNewPart
¶ Adds new part for the parent node
Signature
AddParentNewPart(fileName, index, parentNode)
Parameters: - fileName (str) – New fastener assembly parent node name NOTE: The full Unicode character set is not supported for this parameter.
- index (int) – The hole index in the fastener assembly
- parentNode (bool) – Whether the fastener assembly node is parent
New in version NX9.0.0.
License requirements: None.
AddRemovalHoleIndex¶
-
FastenerAssy.
AddRemovalHoleIndex
¶ Add the removal hole index in the fastener setup data
Signature
AddRemovalHoleIndex(index)
Parameters: index (int) – The hole index in the fastener assembly to be removed New in version NX9.0.0.
License requirements: None.
AddScrewArray¶
-
FastenerAssy.
AddScrewArray
¶ Adds stack array
Signature
AddScrewArray(krxFile, lengthMatch, libPath, libName, fullPath, index, type)
Parameters: - krxFile (str) – The krx file of the stack NOTE: The full Unicode character set is not supported for this parameter.
- lengthMatch (str) – The length match from fastener data and given node NOTE: The full Unicode character set is not supported for this parameter.
- libPath (str) – Ask fastener library path NOTE: The full Unicode character set is not supported for this parameter.
- libName (str) – Ask fastener library name NOTE: The full Unicode character set is not supported for this parameter.
- fullPath (str) – Stack file full path NOTE: The full Unicode character set is not supported for this parameter.
- index (int) – The hole index in the fastener assembly
- type (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – The stack type method
New in version NX9.0.0.
License requirements: None.
AddTopNode¶
-
FastenerAssy.
AddTopNode
¶ Adds top node for the fastener assembly
Signature
AddTopNode(point, direction, selObject, index)
Parameters: - point (
NXOpen.Point3d
) – The point of the fastener to assemble - direction (
NXOpen.Point3d
) – The direciton of the fastener to assemble - selObject (
NXOpen.NXObject
) – The default cylindrical face of the hole data, selObject type should be FACE - index (int) – The hole index in the fastener assembly
Returns: Output the instance of the parent node
Return type: New in version NX9.0.0.
License requirements: None.
- point (
AdjustFastenerLength¶
-
FastenerAssy.
AdjustFastenerLength
¶ Adjusts the fastener assembly length
Signature
AdjustFastenerLength(parentIndex, childIndex, nodeType)
Parameters: - parentIndex (int) – parent index
- childIndex (int) – child index
- nodeType (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – the stack type method
New in version NX9.0.0.
License requirements: None.
CreateArrayHole¶
-
FastenerAssy.
CreateArrayHole
¶ Creates array hole data for the fastener assembly
Signature
CreateArrayHole(index)
Parameters: index (int) – the hole index in the fastener assembly New in version NX9.0.0.
License requirements: None.
CreateFastenerConstraints¶
-
FastenerAssy.
CreateFastenerConstraints
¶ Creates fastener assembly constraint
Signature
CreateFastenerConstraints(index)
Parameters: index (int) – the hole index in the fastener assembly to create constraints New in version NX9.0.0.
License requirements: None.
CreateReusableBuilder¶
-
FastenerAssy.
CreateReusableBuilder
¶ Creates new reusable builder
Signature
CreateReusableBuilder(parentIndex, childIndex, nodeType)
Parameters: - parentIndex (int) – parent node index in the fastener assembly
- childIndex (int) – child node index in the fastener assembly
- nodeType (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – the stack type method
Returns: the new
NXOpen.Tooling.AddReusablePart
instanceReturn type: New in version NX9.0.0.
License requirements: None.
CreateReusablePocket¶
-
FastenerAssy.
CreateReusablePocket
¶ Creates reusable pocket
Signature
CreateReusablePocket(commit)
Parameters: commit (bool) – whether to create pocket New in version NX9.0.0.
License requirements: None.
CreateSameAssemblyData¶
-
FastenerAssy.
CreateSameAssemblyData
¶ Creates the same assembly data type
Signature
CreateSameAssemblyData(addedIndex, index)
Parameters: - addedIndex (int) – find the the hole index with the same parameter and node type in the fastener assembly
- index (int) – the hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
DeleteArrayHole¶
-
FastenerAssy.
DeleteArrayHole
¶ Deletes array hole data for the fastener assembly
Signature
DeleteArrayHole(index)
Parameters: index (int) – the hole index in the fastener assembly New in version NX9.0.0.
License requirements: None.
DeleteReusablePocket¶
-
FastenerAssy.
DeleteReusablePocket
¶ Deletes reusable pocket
Signature
DeleteReusablePocket()
New in version NX9.0.0.
License requirements: None.
EraseAssemblyData¶
-
FastenerAssy.
EraseAssemblyData
¶ Erases the assembly data
Signature
EraseAssemblyData(parentIndex)
Parameters: parentIndex (int) – parent index New in version NX9.0.0.
License requirements: None.
EraseFastenerAssembly¶
-
FastenerAssy.
EraseFastenerAssembly
¶ Erases fastener assembly
Signature
EraseFastenerAssembly(parentInx, removeParent, removeScrew, removeStack, removeArray, removeBuilder, initscrewBuilder, initstackBuilder, removeData)
Parameters: - parentInx (int) – parent index
- removeParent (bool) – whether to remove parent instance
- removeScrew (bool) – whether to remove screw
- removeStack (bool) – whether to remove top stack and bottom stack
- removeArray (bool) – whether to remove component array
- removeBuilder (bool) – whether to remove builder
- initscrewBuilder (bool) – whether to initialize screw builder
- initstackBuilder (bool) – whether to initialize stack builder
- removeData (bool) – whether to remove data
New in version NX9.0.0.
License requirements: None.
EraseFastenerAssemblyData¶
-
FastenerAssy.
EraseFastenerAssemblyData
¶ Erases the fastener assembly data, including the hole data and assembly data in the fastener setup data
Signature
EraseFastenerAssemblyData(index)
Parameters: index (int) – The hole index in the fastener assembly to be removed New in version NX9.0.0.
License requirements: None.
EraseFastenerSetupData¶
-
FastenerAssy.
EraseFastenerSetupData
¶ Erases the data (hole and assembly data) in fastener assembly
Signature
EraseFastenerSetupData()
New in version NX9.0.0.
License requirements: None.
EraseStackArray¶
-
FastenerAssy.
EraseStackArray
¶ Erases stack array
Signature
EraseStackArray(parentIndex, inx, type)
Parameters: - parentIndex (int) – Parent index
- inx (int) – Child index
- type (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – The stack type method
New in version NX9.0.0.
License requirements: None.
GetFastenerMode¶
-
FastenerAssy.
GetFastenerMode
¶ Gets the fastener mode
Signature
GetFastenerMode()
Returns: Return type: NXOpen.Tooling.FastenerAssyModeMethod
New in version NX9.0.0.
License requirements: None.
GetFastenerSelectionType¶
-
FastenerAssy.
GetFastenerSelectionType
¶ Gets the selection type for the hole in the fastener assembly
Signature
GetFastenerSelectionType()
Returns: The selection type to add the fastener assembly Return type: NXOpen.Tooling.FastenerAssySelectionTypeMethod
New in version NX9.0.0.
License requirements: None.
GetReusablePocketBuilder¶
-
FastenerAssy.
GetReusablePocketBuilder
¶ Gets the reusable pocket builder
Signature
GetReusablePocketBuilder()
Returns: The reusable component pocket builder Return type: NXOpen.Tooling.ReusablePocketBuilder
New in version NX9.0.0.
License requirements: None.
InitPocketBuilder¶
-
FastenerAssy.
InitPocketBuilder
¶ Inits pocket builder
Signature
InitPocketBuilder()
New in version NX9.0.0.
License requirements: None.
ReadAssemblyConfigure¶
-
FastenerAssy.
ReadAssemblyConfigure
¶ Reads fastener assembly configuration data from the hole data
Signature
ReadAssemblyConfigure(holeNum, partOcc)
Parameters: - holeNum (int) – hole num
- partOcc (
NXOpen.Assemblies.Component
) – parent node part occurance
New in version NX9.0.0.
License requirements: None.
RemoveFastenerConstraints¶
-
FastenerAssy.
RemoveFastenerConstraints
¶ Removes fastener assembly constraint
Signature
RemoveFastenerConstraints(index)
Parameters: index (int) – the hole index in the fastener assembly to delete constraints New in version NX9.0.0.
License requirements: None.
RemoveSelectedHole¶
-
FastenerAssy.
RemoveSelectedHole
¶ Removes the selected hole from the fastener setup data
Signature
RemoveSelectedHole()
New in version NX9.0.0.
License requirements: None.
RenameParentNode¶
-
FastenerAssy.
RenameParentNode
¶ Renames the parent node
Signature
RenameParentNode(index, newname)
Parameters: - index (int) – parent node index in fastener assembly
- newname (str) – new name for the parent node NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: None.
SaveUdoData¶
-
FastenerAssy.
SaveUdoData
¶ Saves UDO data for fastener assembly
Signature
SaveUdoData()
New in version NX9.0.0.
License requirements: None.
SelectScrewSize¶
-
FastenerAssy.
SelectScrewSize
¶ Selects the screw size
Signature
SelectScrewSize(inx, diameter, origindiameter, selDiameter)
Parameters: - inx (int) – parent index
- diameter (float) – diameter in hole data
- origindiameter (float) – origin diameter in hole data
- selDiameter (bool) – whether to select diameter
New in version NX9.0.0.
License requirements: None.
SetAssemblyExtentLength¶
-
FastenerAssy.
SetAssemblyExtentLength
¶ Sets the extent length for the fastener assembly data
Signature
SetAssemblyExtentLength(index, extentLength)
Parameters: - index (int) – hole index in fastener assembly
- extentLength (float) – The extent Length of the fastener assembly
New in version NX9.0.0.
License requirements: None.
SetBlindHole¶
-
FastenerAssy.
SetBlindHole
¶ Sets the blind hole for the hole in the fastener assembly
Signature
SetBlindHole(inx, blindhole)
Parameters: - inx (int) – parent index
- blindhole (bool) – whether the hole is blind hole
New in version NX10.0.0.
License requirements: None.
SetCreatePocket¶
-
FastenerAssy.
SetCreatePocket
¶ Sets the flag to indicate whether to create pocket when adding the fastener
Signature
SetCreatePocket(create)
Parameters: create (bool) – Whether the fastener assembly is created pocket New in version NX9.0.0.
License requirements: None.
SetDefaultPlanarFaces¶
-
FastenerAssy.
SetDefaultPlanarFaces
¶ Sets the default planar face for the hole in the fastener assembly
Signature
SetDefaultPlanarFaces(defaultPlanarFace, inx)
Parameters: - defaultPlanarFace (
NXOpen.NXObject
) – The default planar face of the hole data, defaultPlanarFace type should be FACE - inx (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- defaultPlanarFace (
SetFastenerExtentLength¶
-
FastenerAssy.
SetFastenerExtentLength
¶ Sets the extent length for the hole in the fastener assembly
Signature
SetFastenerExtentLength(extentLength)
Parameters: extentLength (float) – The extent Length of the fastener assembly New in version NX9.0.0.
License requirements: None.
SetFastenerMode¶
-
FastenerAssy.
SetFastenerMode
¶ Sets the fastener mode
Signature
SetFastenerMode(modeMethod)
Parameters: modeMethod ( NXOpen.Tooling.FastenerAssyModeMethod
) –New in version NX9.0.0.
License requirements: None.
SetFastenerSelectionType¶
-
FastenerAssy.
SetFastenerSelectionType
¶ Sets the selection type for the hole in the fastener assembly
Signature
SetFastenerSelectionType(selectionType)
Parameters: selectionType ( NXOpen.Tooling.FastenerAssySelectionTypeMethod
) – The selection type to add the fastener assemblyNew in version NX9.0.0.
License requirements: None.
SetHoleDefaultCylindricalFace¶
-
FastenerAssy.
SetHoleDefaultCylindricalFace
¶ Sets the default cylindrical face for the hole in the fastener assembly
Signature
SetHoleDefaultCylindricalFace(defaultCylFaces, index)
Parameters: - defaultCylFaces (
NXOpen.NXObject
) – The default cylindrical faces of the hole data, defaultCylFaces type should be FACE - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- defaultCylFaces (
SetHoleDiameter¶
-
FastenerAssy.
SetHoleDiameter
¶ Sets the diameter for the hole in the fastener assembly
Signature
SetHoleDiameter(diameter, index)
Parameters: - diameter (float) – The diameter of the hole data
- index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
SetHoleDirection¶
-
FastenerAssy.
SetHoleDirection
¶ Sets the direction for the hole in the fastener assembly
Signature
SetHoleDirection(direction, index)
Parameters: - direction (
NXOpen.Point3d
) – The direcion of the hole data - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- direction (
SetHoleFaces¶
-
FastenerAssy.
SetHoleFaces
¶ Sets the faces for the hole in the fastener assembly
Signature
SetHoleFaces(holeFace, index)
Parameters: - holeFace (
NXOpen.NXObject
) – The hole face of the hole data, holeFace type is FACE - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- holeFace (
SetHoleHeight¶
-
FastenerAssy.
SetHoleHeight
¶ Sets the height for the hole in the fastener assembly
Signature
SetHoleHeight(height, index)
Parameters: - height (float) – The height of the hole data
- index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
SetHoleOriginDiameter¶
-
FastenerAssy.
SetHoleOriginDiameter
¶ Sets the origin diameter for the hole in the fastener assembly
Signature
SetHoleOriginDiameter(originDiameter, index)
Parameters: - originDiameter (float) – The origin diameter of the hole data
- index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
SetHoleOriginHeight¶
-
FastenerAssy.
SetHoleOriginHeight
¶ Sets the origin height for the hole in the fastener assembly
Signature
SetHoleOriginHeight(originheight, index)
Parameters: - originheight (float) – The origin height of the hole data
- index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
SetHoleOriginPosition¶
-
FastenerAssy.
SetHoleOriginPosition
¶ Sets the origin position for the hole in the fastener assembly
Signature
SetHoleOriginPosition(originposition, index)
Parameters: - originposition (
NXOpen.Point3d
) – The origin position of the hole data - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- originposition (
SetHolePosition¶
-
FastenerAssy.
SetHolePosition
¶ Sets the position for the hole in the fastener assembly
Signature
SetHolePosition(position, index)
Parameters: - position (
NXOpen.Point3d
) – The position of the hole data - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- position (
SetHoleSideCylindricalFaces¶
-
FastenerAssy.
SetHoleSideCylindricalFaces
¶ Sets the side cylindrical faces for the hole in the fastener assembly
Signature
SetHoleSideCylindricalFaces(sideCylFace, index)
Parameters: - sideCylFace (
NXOpen.NXObject
) – The side cylinderical Face of the hole data - index (int) – The hole index in the fastener assembly, sideCylFace type should be FACE
New in version NX9.0.0.
License requirements: None.
- sideCylFace (
SetInstanceFeatureFaces¶
-
FastenerAssy.
SetInstanceFeatureFaces
¶ Sets the instance feature face for the hole in the fastener assembly
Signature
SetInstanceFeatureFaces(instanceFeature, inx)
Parameters: - instanceFeature (
NXOpen.NXObject
) – The instance feature face of the hole data, instanceFeature type should be FACE - inx (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- instanceFeature (
SetItemName¶
-
FastenerAssy.
SetItemName
¶ Adds item description for the part
Signature
SetItemName(partName, itemName)
Parameters: - partName (str) – The part name
- itemName (str) – Item name
New in version NX9.0.0.
License requirements: None.
SetReusablePocketBuilder¶
-
FastenerAssy.
SetReusablePocketBuilder
¶ Sets the reusable pocket builder
Signature
SetReusablePocketBuilder(pocketTag)
Parameters: pocketTag ( NXOpen.Tooling.ReusablePocketBuilder
) – The reusable component pocket builderNew in version NX9.0.0.
License requirements: None.
SetReuseBuilder¶
-
FastenerAssy.
SetReuseBuilder
¶ Sets the reuse builder
Signature
SetReuseBuilder(index, nodeType, childIndex, partOcc)
Parameters: - index (int) – parent node index in fastener assembly
- nodeType (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – the stack type method - childIndex (int) – child hole index in fastener assembly
- partOcc (
NXOpen.Assemblies.Component
) – new part occruance
New in version NX9.0.0.
License requirements: None.
SetSidePlanarFaces¶
-
FastenerAssy.
SetSidePlanarFaces
¶ Sets the side planar faces for the hole in the fastener assembly
Signature
SetSidePlanarFaces(sidePlanarFace, index)
Parameters: - sidePlanarFace (
NXOpen.NXObject
) – The side planar face of the hole data, sidePlanarFace type should be FACE - index (int) – The hole index in the fastener assembly
New in version NX9.0.0.
License requirements: None.
- sidePlanarFace (
SubstituteFastenerStack¶
-
FastenerAssy.
SubstituteFastenerStack
¶ Substitutes fastener stack
Signature
SubstituteFastenerStack(parentIndex, childIndex, nodeType, partFile, krxFile, libName, pathInLib, lengthMatch, fullPath)
Parameters: - parentIndex (int) – parent node index in the fastener assembly
- childIndex (int) – child node index in the fastener assembly
- nodeType (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – the stack type method - partFile (str) – part file NOTE: The full Unicode character set is not supported for this parameter.
- krxFile (str) – krx file NOTE: The full Unicode character set is not supported for this parameter.
- libName (str) – library name NOTE: The full Unicode character set is not supported for this parameter.
- pathInLib (str) – library path NOTE: The full Unicode character set is not supported for this parameter.
- lengthMatch (str) – the length match from fastener data and given node NOTE: The full Unicode character set is not supported for this parameter.
- fullPath (str) – screw file full path NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: None.
UpdateDefaultStandard¶
-
FastenerAssy.
UpdateDefaultStandard
¶ Updates default standard hole data for the fastener assembly configuration
Signature
UpdateDefaultStandard(index, standard, form, type)
Parameters: - index (int) – The hole index in hole map data
- standard (str) – The default hole standard type in the assembly configuration NOTE: The full Unicode character set is not supported for this parameter.
- form (str) – The default hole form in the assembly configuration NOTE: The full Unicode character set is not supported for this parameter.
- type (str) – The default hole screw type in the assembly configuration NOTE: The full Unicode character set is not supported for this parameter.
New in version NX9.0.0.
License requirements: None.
UpdateFastenerLength¶
-
FastenerAssy.
UpdateFastenerLength
¶ Updates the fastener length
Signature
UpdateFastenerLength(adjustLength)
Parameters: adjustLength (bool) – Whether to adjust length in the fastener assembly New in version NX9.0.0.
License requirements: None.
UpdateFastenerStacks¶
-
FastenerAssy.
UpdateFastenerStacks
¶ Updates fastener stacks
Signature
UpdateFastenerStacks(parentIndex, updateScrew, updatePocket)
Parameters: - parentIndex (int) – parent index
- updateScrew (bool) – whether to update screw
- updatePocket (bool) – whether to update pocket
New in version NX9.0.0.
License requirements: None.
UpdateHoleData¶
-
FastenerAssy.
UpdateHoleData
¶ Updates the hole data
Signature
UpdateHoleData(inx, originheight, originPoint, threadhole, blindhole)
Parameters: - inx (int) – parent index
- originheight (float) – origin height in hole data
- originPoint (
NXOpen.Point3d
) – origin point in hole data - threadhole (bool) – whether the hole is thread hole
- blindhole (bool) – whether the hole is blind hole
New in version NX9.0.0.
License requirements: None.
UpdateHolePostion¶
-
FastenerAssy.
UpdateHolePostion
¶ Updates the hole positon for position method
Signature
UpdateHolePostion(parentIndex, dirOne, tempPnt, pointOne, height, orignHeight, offSetDistance)
Parameters: - parentIndex (int) – parent node index
- dirOne (
NXOpen.Point3d
) – direction in hole data - tempPnt (
NXOpen.Point3d
) – position in hole data - pointOne (
NXOpen.Point3d
) – origin position in hole data - height (float) – height in hole data
- orignHeight (float) – origin height in hole data
- offSetDistance (float) – offset distance in hole data
New in version NX9.0.0.
License requirements: None.
UpdateStackPosition¶
-
FastenerAssy.
UpdateStackPosition
¶ Updates the fastener assembly after changing stacks or changing stack properties
Signature
UpdateStackPosition(parentIndex, childIndex, nodeType, deltaLength)
Parameters: - parentIndex (int) – parent index
- childIndex (int) – child index
- nodeType (
NXOpen.Tooling.FastenerAssyStackTypeMethod
) – node type - deltaLength (float) – the stack length to be changed
New in version NX9.0.0.
License requirements: None.
UpdateTopBottomStacks¶
-
FastenerAssy.
UpdateTopBottomStacks
¶ Updates fastener assembly according to the new extends
Signature
UpdateTopBottomStacks(index, type, isSameFace, face)
Parameters: - index (int) – parent node index in fastener assembly
- type (
NXOpen.Tooling.FastenerAssySelectionObjectMethod
) – top object or bottom object type - isSameFace (bool) – whether the fastener assembly is same face
- face (
NXOpen.NXObject
) – top or bottom face
New in version NX9.0.0.
License requirements: None.
Validate¶
-
FastenerAssy.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.