FaceSplitBuilder Class¶
-
class
NXOpen.Tooling.
FaceSplitBuilder
¶ Bases:
NXOpen.Builder
Represents a face split operation
To create a new instance of this class, use
NXOpen.Tooling.FaceSplitCollection.CreateFaceSplitBuilder
Default values.
Property Value Tolerance 0.025 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DivObjects | Returns the dividing objects which will be different according to the split type |
FaceToDivide | Returns the faces to be divided |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance is used to do dividing face operation |
Type | Returns or sets the split face type which splits a face by using curves, edges, plane, face, isolines or intersected curves with another body |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateIsoclines | Create isocline |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FindMoldUnsplitFace | Set the reference point to the selected face center. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FaceSplitBuilderFaceSplitType Enumeration | the type for Split Face |
Property Detail¶
DivObjects¶
-
FaceSplitBuilder.
DivObjects
¶ Returns the dividing objects which will be different according to the split type
-------------------------------------
Getter Method
Signature
DivObjects()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
FaceToDivide¶
-
FaceSplitBuilder.
FaceToDivide
¶ Returns the faces to be divided
-------------------------------------
Getter Method
Signature
FaceToDivide()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
Tolerance¶
-
FaceSplitBuilder.
Tolerance
¶ Returns or sets the tolerance is used to do dividing face operation
-------------------------------------
Getter Method
Signature
Tolerance()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance(tolerance)
Parameters: tolerance (float) – New in version NX7.5.0.
License requirements: None.
Type¶
-
FaceSplitBuilder.
Type
¶ Returns or sets the split face type which splits a face by using curves, edges, plane, face, isolines or intersected curves with another body
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.FaceSplitBuilderFaceSplitType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(splitType)
Parameters: splitType ( NXOpen.Tooling.FaceSplitBuilderFaceSplitType
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateIsoclines¶
-
FaceSplitBuilder.
CreateIsoclines
¶ Create isocline
Signature
CreateIsoclines(pFacesToDivide)
Parameters: pFacesToDivide (list of NXOpen.Face
) – faces to be divided with isoclinesReturns: isoclines on selected faces Return type: list of NXOpen.Curve
New in version NX7.5.0.
License requirements: None.
FindMoldUnsplitFace¶
-
FaceSplitBuilder.
FindMoldUnsplitFace
¶ Set the reference point to the selected face center.
Signature
FindMoldUnsplitFace()
New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR nx_electrode_wizard (“NX Electrode Wizard”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Validate¶
-
FaceSplitBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.