ElectrodeInitializationBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeInitializationBuilder
¶ Bases:
NXOpen.Builder
Electrode initialize project builder to creates an electrode design assembly.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateProjectBuilder
Default values.
Property Value Rename 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CurrentMset | Returns or sets the machine set part which is the working part. |
Face | Returns the face whose center will be the origin of the machine set csys. |
InputName | Returns or sets the input name as project name. |
PathBrowser | Returns or sets the path browser. |
Rename | Returns or sets the component name can be defined in the part name management. |
Tag | Returns the Tag for this object. |
Workpiece | Returns the utility to get the workpiece to create an electrode design project. |
WorkpieceList | Returns the utility to get the workpiece list to create an electrode design project. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateCloneObjectOfMsetPart | Creates clone object of machine set part. |
CreateCloneObjectOfTopPart | Creates clone object of top part. |
CreateCloneObjectOfWorkingPart | Creates clone object of working part. |
CreateMsetPart | Creates the mset part. |
CreateProject | Creates the assembly structure of Electrode Wizard project. |
CreateWorkingPart | Creates the working part. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisposeCloneObject | Disposes the clone object. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetWorkingPart | Gets the working part in mset. |
InitLinkObjects | Links the selected objects to the working component of Electrode assembly. |
SetMsetCsysMatrixOrigin | Sets csys matrix and origin. |
SetMsetCsysOriginToFaceCenter | Sets MSET CSYS origin to center of the selected faces. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurrentMset¶
-
ElectrodeInitializationBuilder.
CurrentMset
¶ Returns or sets the machine set part which is the working part.
-------------------------------------
Getter Method
Signature
CurrentMset()
Returns: machine set part Return type: NXOpen.TaggedObject
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
CurrentMset(mset)
Parameters: mset ( NXOpen.TaggedObject
) – machine set partNew in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Face¶
-
ElectrodeInitializationBuilder.
Face
¶ Returns the face whose center will be the origin of the machine set csys.
-------------------------------------
Getter Method
Signature
Face()
Returns: Return type: NXOpen.SelectFace
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
InputName¶
-
ElectrodeInitializationBuilder.
InputName
¶ Returns or sets the input name as project name.
-------------------------------------
Getter Method
Signature
InputName()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
InputName(inputName)
Parameters: inputName (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
PathBrowser¶
-
ElectrodeInitializationBuilder.
PathBrowser
¶ Returns or sets the path browser.
-------------------------------------
Getter Method
Signature
PathBrowser()
Returns: Return type: str New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
PathBrowser(foldername)
Parameters: foldername (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Rename¶
-
ElectrodeInitializationBuilder.
Rename
¶ Returns or sets the component name can be defined in the part name management.
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Workpiece¶
-
ElectrodeInitializationBuilder.
Workpiece
¶ Returns the utility to get the workpiece to create an electrode design project.
-------------------------------------
Getter Method
Signature
Workpiece()
Returns: Return type: NXOpen.SelectBody
New in version NX8.0.0.
License requirements: None.
WorkpieceList¶
-
ElectrodeInitializationBuilder.
WorkpieceList
¶ Returns the utility to get the workpiece list to create an electrode design project.
-------------------------------------
Getter Method
Signature
WorkpieceList()
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.5.3.
License requirements: None.
Method Detail¶
CreateCloneObjectOfMsetPart¶
-
ElectrodeInitializationBuilder.
CreateCloneObjectOfMsetPart
¶ Creates clone object of machine set part.
Signature
CreateCloneObjectOfMsetPart()
Returns: Return type: NXOpen.Tooling.CloneObject
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CreateCloneObjectOfTopPart¶
-
ElectrodeInitializationBuilder.
CreateCloneObjectOfTopPart
¶ Creates clone object of top part.
Signature
CreateCloneObjectOfTopPart()
Returns: Return type: NXOpen.Tooling.CloneObject
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CreateCloneObjectOfWorkingPart¶
-
ElectrodeInitializationBuilder.
CreateCloneObjectOfWorkingPart
¶ Creates clone object of working part.
Signature
CreateCloneObjectOfWorkingPart()
Returns: Return type: NXOpen.Tooling.CloneObject
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CreateMsetPart¶
-
ElectrodeInitializationBuilder.
CreateMsetPart
¶ Creates the mset part.
Signature
CreateMsetPart(cloneObject)
Parameters: cloneObject ( NXOpen.Tooling.CloneObject
) –Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CreateProject¶
-
ElectrodeInitializationBuilder.
CreateProject
¶ Creates the assembly structure of Electrode Wizard project.
Signature
CreateProject(cloneObject)
Parameters: cloneObject ( NXOpen.Tooling.CloneObject
) –New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
CreateWorkingPart¶
-
ElectrodeInitializationBuilder.
CreateWorkingPart
¶ Creates the working part.
Signature
CreateWorkingPart(cloneObject, msetPartTag)
Parameters: - cloneObject (
NXOpen.Tooling.CloneObject
) – - msetPartTag (
NXOpen.TaggedObject
) –
Returns: Return type: New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
- cloneObject (
DisposeCloneObject¶
-
ElectrodeInitializationBuilder.
DisposeCloneObject
¶ Disposes the clone object.
Signature
DisposeCloneObject(cloneObject)
Parameters: cloneObject ( NXOpen.Tooling.CloneObject
) –New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
GetWorkingPart¶
-
ElectrodeInitializationBuilder.
GetWorkingPart
¶ Gets the working part in mset.
Signature
GetWorkingPart(msetPartTag)
Parameters: msetPartTag ( NXOpen.TaggedObject
) –Returns: Return type: NXOpen.TaggedObject
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
InitLinkObjects¶
-
ElectrodeInitializationBuilder.
InitLinkObjects
¶ Links the selected objects to the working component of Electrode assembly.
Signature
InitLinkObjects(workingPartTag)
Parameters: workingPartTag ( NXOpen.TaggedObject
) –New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
SetMsetCsysMatrixOrigin¶
-
ElectrodeInitializationBuilder.
SetMsetCsysMatrixOrigin
¶ Sets csys matrix and origin.
Signature
SetMsetCsysMatrixOrigin(matrix, origin)
Parameters: - matrix (
NXOpen.Matrix3x3
) – csys matrix - origin (
NXOpen.Point3d
) – csys origin
New in version NX8.5.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
- matrix (
SetMsetCsysOriginToFaceCenter¶
-
ElectrodeInitializationBuilder.
SetMsetCsysOriginToFaceCenter
¶ Sets MSET CSYS origin to center of the selected faces.
Signature
SetMsetCsysOriginToFaceCenter()
New in version NX9.0.1.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Validate¶
-
ElectrodeInitializationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.