ElectrodeDeleteBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeDeleteBuilder
¶ Bases:
NXOpen.Builder
Electrode delete component builder to remove blank, pallet and holder from assembly.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateDeleteComponentBuilder
Default values.
Property Value KeepSize 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Component | Returns the utility to get component to delete. |
Head | Returns the utility to get sparking solid to delete. |
KeepSize | Returns or sets the option to keep blank size after deleting sparking solid. |
RoundPosition | Returns or sets the option to round electrode position. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the object type to be deleted. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElectrodeDeleteBuilderTypes Enumeration | delete sparking solid from blank or delete blank, pallet or holder directly. |
Property Detail¶
Component¶
-
ElectrodeDeleteBuilder.
Component
¶ Returns the utility to get component to delete.
-------------------------------------
Getter Method
Signature
Component()
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Head¶
-
ElectrodeDeleteBuilder.
Head
¶ Returns the utility to get sparking solid to delete.
-------------------------------------
Getter Method
Signature
Head()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
KeepSize¶
-
ElectrodeDeleteBuilder.
KeepSize
¶ Returns or sets the option to keep blank size after deleting sparking solid.
-------------------------------------
Getter Method
Signature
KeepSize()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
KeepSize(keepSize)
Parameters: keepSize (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
RoundPosition¶
-
ElectrodeDeleteBuilder.
RoundPosition
¶ Returns or sets the option to round electrode position.
-------------------------------------
Getter Method
Signature
RoundPosition()
Returns: Return type: bool New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
RoundPosition(roundPosition)
Parameters: roundPosition (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Type¶
-
ElectrodeDeleteBuilder.
Type
¶ Returns or sets the object type to be deleted.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.ElectrodeDeleteBuilderTypes
New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.ElectrodeDeleteBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Method Detail¶
Validate¶
-
ElectrodeDeleteBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.