ElectrodeCopyBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeCopyBuilder
¶ Bases:
NXOpen.Builder
The ElectrodeCopy builder
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeCopyCollection.CreateElectrodeCopyBuilder
Default values.
Property Value DefNum 1 SelType Transform New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CopyInstance | Returns or sets the setting indicates the copy is a new part or an instance. |
DefNum | Returns or sets the number of transform |
MirrorPlane | Returns the mirror plane |
Rename | Returns or sets the new electrode name |
SelToFace | Returns the selected ‘to’ face |
SelType | Returns or sets the copy type |
SelectElectrode | Returns the selected electrode |
SelectFromFace | Returns the selected ‘from’ face |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElectrodeCopyBuilderCopy Enumeration | Represents an index to copy type |
Property Detail¶
CopyInstance¶
-
ElectrodeCopyBuilder.
CopyInstance
¶ Returns or sets the setting indicates the copy is a new part or an instance.
-------------------------------------
Getter Method
Signature
CopyInstance()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CopyInstance(copyInstance)
Parameters: copyInstance (bool) – New in version NX7.5.0.
License requirements: None.
DefNum¶
-
ElectrodeCopyBuilder.
DefNum
¶ Returns or sets the number of transform
-------------------------------------
Getter Method
Signature
DefNum()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefNum(defNum)
Parameters: defNum (int) – New in version NX6.0.0.
License requirements: None.
MirrorPlane¶
-
ElectrodeCopyBuilder.
MirrorPlane
¶ Returns the mirror plane
-------------------------------------
Getter Method
Signature
MirrorPlane()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Rename¶
-
ElectrodeCopyBuilder.
Rename
¶ Returns or sets the new electrode name
-------------------------------------
Getter Method
Signature
Rename()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Rename(rename)
Parameters: rename (bool) – New in version NX6.0.0.
License requirements: None.
SelToFace¶
-
ElectrodeCopyBuilder.
SelToFace
¶ Returns the selected ‘to’ face
-------------------------------------
Getter Method
Signature
SelToFace()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SelType¶
-
ElectrodeCopyBuilder.
SelType
¶ Returns or sets the copy type
-------------------------------------
Getter Method
Signature
SelType()
Returns: Return type: NXOpen.Tooling.ElectrodeCopyBuilderCopy
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelType(selType)
Parameters: selType ( NXOpen.Tooling.ElectrodeCopyBuilderCopy
) –New in version NX6.0.0.
License requirements: None.
SelectElectrode¶
-
ElectrodeCopyBuilder.
SelectElectrode
¶ Returns the selected electrode
-------------------------------------
Getter Method
Signature
SelectElectrode()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
SelectFromFace¶
-
ElectrodeCopyBuilder.
SelectFromFace
¶ Returns the selected ‘from’ face
-------------------------------------
Getter Method
Signature
SelectFromFace()
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ElectrodeCopyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.