ElectrodeBlankBuilderBlankMaterial Enumeration¶
NXOpen.Tooling.ElectrodeBlankBuilder.BlankMaterial is an alias for NXOpen.Tooling.ElectrodeBlankBuilderBlankMaterial
-
class
NXOpen.Tooling.
ElectrodeBlankBuilderBlankMaterial
¶ Bases:
object
Represents the blank material option.
Enum Members
Enum Member Enum Member Description Copper the material of the blank is copperGraphite the material of the blank is graphite-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-