EjectorPostProcessingBuilder Class¶
-
class
NXOpen.Tooling.
EjectorPostProcessingBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create Mold Wizard ejector post processing.
To create a new instance of this class, use
NXOpen.Tooling.EjectorPostProcessingCollection.CreateEjectorPostProcessingBuilder
Default values.
Property Value ActionType AdjustLength TrimPart Notrimpart TrimSurface Face New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ActionType | Returns or sets the trim method of ejector pin post processing. |
FitDistance | Returns the distance used to adjust the length of an ejector pin for the false body |
OffsetValue | Returns the offset value is used to create offset feature on the trimmed ejector pin true body. |
Tag | Returns the Tag for this object. |
TargetComponents | Returns the target components which contains the target ejector pins to be trimmed. |
ToolFace | Returns the faces used to trim an ejector pin. |
ToolSheetBody | Returns the sheet body used to trim an ejector pin. |
TrimPart | Returns or sets the trim part in which trim surface features are cycled. |
TrimSurface | Returns or sets the trim surface used to trim an ejector pin. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetTrimDataDetails | Set details of the trim data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
EjectorPostProcessingBuilderTrimMethod Enumeration | The processing type: Trim, Adjust length and Untrim. |
EjectorPostProcessingBuilderTrimPartName Enumeration | The trim part where to find a trim surface as tool to trim ejector pins. |
EjectorPostProcessingBuilderTrimSufaceName Enumeration | The trim surface types. |
Property Detail¶
ActionType¶
-
EjectorPostProcessingBuilder.
ActionType
¶ Returns or sets the trim method of ejector pin post processing.
-------------------------------------
Getter Method
Signature
ActionType()
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ActionType(actionType)
Parameters: actionType ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimMethod
) –New in version NX7.5.0.
License requirements: None.
FitDistance¶
-
EjectorPostProcessingBuilder.
FitDistance
¶ Returns the distance used to adjust the length of an ejector pin for the false body
-------------------------------------
Getter Method
Signature
FitDistance()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
OffsetValue¶
-
EjectorPostProcessingBuilder.
OffsetValue
¶ Returns the offset value is used to create offset feature on the trimmed ejector pin true body.
-------------------------------------
Getter Method
Signature
OffsetValue()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
TargetComponents¶
-
EjectorPostProcessingBuilder.
TargetComponents
¶ Returns the target components which contains the target ejector pins to be trimmed.
-------------------------------------
Getter Method
Signature
TargetComponents()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
ToolFace¶
-
EjectorPostProcessingBuilder.
ToolFace
¶ Returns the faces used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
ToolFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
ToolSheetBody¶
-
EjectorPostProcessingBuilder.
ToolSheetBody
¶ Returns the sheet body used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
ToolSheetBody()
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
TrimPart¶
-
EjectorPostProcessingBuilder.
TrimPart
¶ Returns or sets the trim part in which trim surface features are cycled.
-------------------------------------
Getter Method
Signature
TrimPart()
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimPartName
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimPart(trimPart)
Parameters: trimPart ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimPartName
) –New in version NX7.5.0.
License requirements: None.
TrimSurface¶
-
EjectorPostProcessingBuilder.
TrimSurface
¶ Returns or sets the trim surface used to trim an ejector pin.
-------------------------------------
Getter Method
Signature
TrimSurface()
Returns: Return type: NXOpen.Tooling.EjectorPostProcessingBuilderTrimSufaceName
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimSurface(trimSurface)
Parameters: trimSurface ( NXOpen.Tooling.EjectorPostProcessingBuilderTrimSufaceName
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetTrimDataDetails¶
-
EjectorPostProcessingBuilder.
SetTrimDataDetails
¶ Set details of the trim data.
Signature
SetTrimDataDetails(surfaceType, targets, tools)
Parameters: - surfaceType (int) – the surface type.
- targets (list of
NXOpen.NXObject
) – array of target ejector pins. - tools (list of
NXOpen.NXObject
) – array of tool objects.
New in version NX7.5.0.
License requirements: None.
Validate¶
-
EjectorPostProcessingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.