EWMultiPositionBuilder Class¶
-
class
NXOpen.Tooling.
EWMultiPositionBuilder
¶ Bases:
NXOpen.Builder
Represents the multiple position builder which is used to get transformed electrode heads together.
To create a new instance of this class, use
NXOpen.Tooling.EWMultiPositionCollection.CreateEwmultiPositionBuilder
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Head | Returns the head to match to another possible head. |
HeadSet | Returns the head sets with specified body and transformation data. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Head¶
-
EWMultiPositionBuilder.
Head
¶ Returns the head to match to another possible head.
-------------------------------------
Getter Method
Signature
Head()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
HeadSet¶
-
EWMultiPositionBuilder.
HeadSet
¶ Returns the head sets with specified body and transformation data.
-------------------------------------
Getter Method
Signature
HeadSet()
Returns: Return type: NXOpen.BodyList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
EWMultiPositionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.