DirectUnfoldBuilderTypes Enumeration¶
NXOpen.Tooling.DirectUnfoldBuilder.Types is an alias for NXOpen.Tooling.DirectUnfoldBuilderTypes
-
class
NXOpen.Tooling.
DirectUnfoldBuilderTypes
¶ Bases:
object
Specifies the option of direct unfold type
Enum Members
Enum Member Enum Member Description Convert the direct unfold type of convert to Sheet MetalMergeBends the direct unfold type of merge bendsDefinePreBends the direct unfold type of define pre-bendsDeleteBends the direct unfold type of delete all bends-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-