DirectUnfoldBuilderMatType Enumeration¶
NXOpen.Tooling.DirectUnfoldBuilder.MatType is an alias for NXOpen.Tooling.DirectUnfoldBuilderMatType
-
class
NXOpen.Tooling.
DirectUnfoldBuilderMatType
¶ Bases:
object
The material database defined in PDW.
It is added in project initialization.
Enum Members
Enum Member Enum Member Description Steel Default is steel.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-