DieBaseBuilderPlatesNumberOpt Enumeration¶
NXOpen.Tooling.DieBaseBuilder.PlatesNumberOpt is an alias for NXOpen.Tooling.DieBaseBuilderPlatesNumberOpt
-
class
NXOpen.Tooling.
DieBaseBuilderPlatesNumberOpt
¶ Bases:
object
plates number options.
Enum Members
Enum Member Enum Member Description PlateFive plates number is 5PlateEight plates number is 8PlateNine plates number is 9PlateTen plates number is 10PlateTwelve plates number is 12-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-