DesignTrimToolBuilder Class¶
-
class
NXOpen.Tooling.
DesignTrimToolBuilder
¶ Bases:
NXOpen.Builder
Represents a builder to be used to create Mold Wizard design trim tool.
To create a new instance of this class, use
NXOpen.Tooling.DesignTrimToolCollection.CreateDesignTrimToolBuilder
Default values.
Property Value NewSurfaceLayer 32 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
NewSurfaceLayer | Returns or sets the layer where the new trim surface is created. |
SourceObject | Returns the face or sheet body. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateDefaultSheet | Create a Moldwizard default trim surface, including CORE_TRIM_SHEET, CAVITY_TRIM_SHEET, CORE_MOLD_SURFACE, CAVITY_MOLD_SURFACE. |
CreateNewComponent | Create a new trim part component in the work part. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetTrimDataDetails | Set details of the trim data. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NewSurfaceLayer¶
-
DesignTrimToolBuilder.
NewSurfaceLayer
¶ Returns or sets the layer where the new trim surface is created.
-------------------------------------
Getter Method
Signature
NewSurfaceLayer()
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewSurfaceLayer(newSurfaceLayer)
Parameters: newSurfaceLayer (int) – New in version NX7.5.0.
License requirements: None.
SourceObject¶
-
DesignTrimToolBuilder.
SourceObject
¶ Returns the face or sheet body.
-------------------------------------
Getter Method
Signature
SourceObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.5.0.
License requirements: None.
Method Detail¶
CreateDefaultSheet¶
-
DesignTrimToolBuilder.
CreateDefaultSheet
¶ Create a Moldwizard default trim surface, including CORE_TRIM_SHEET, CAVITY_TRIM_SHEET, CORE_MOLD_SURFACE, CAVITY_MOLD_SURFACE.
Signature
CreateDefaultSheet(surfaceName, trimPart, sheetType, layer)
Parameters: - surfaceName (str) – the name for the default sheet to create. NOTE: The full Unicode character set is not supported for this parameter.
- trimPart (
NXOpen.NXObject
) – the trim part where to create the default trim surface feature. - sheetType (int) – the sheet type, parting sheet or mold surface.
- layer (int) – the layer to put the new sheet feature.
Returns: the new sheet that is created.
Return type: New in version NX7.5.0.
License requirements: None.
CreateNewComponent¶
-
DesignTrimToolBuilder.
CreateNewComponent
¶ Create a new trim part component in the work part.
Signature
CreateNewComponent(partName, instanceName)
Parameters: - partName (str) – the part name for the new component. NOTE: The full Unicode character set is not supported for this parameter.
- instanceName (str) – the instance name for the new component. NOTE: The full Unicode character set is not supported for this parameter.
Returns: the new component that is created.
Return type: New in version NX7.5.0.
License requirements: None.
SetTrimDataDetails¶
-
DesignTrimToolBuilder.
SetTrimDataDetails
¶ Set details of the trim data.
Signature
SetTrimDataDetails(trimPart, sourceObjectOcc, currentTrimSurfaceName, previousTrimSurfaceName)
Parameters: - trimPart (
NXOpen.NXObject
) – the trim part where to create or edit or trim surface feature. - sourceObjectOcc (
NXOpen.NXObject
) – the source object occurrence used to create a linked feature in the trim part. - currentTrimSurfaceName (str) – the name to set to the trim surface feature. NOTE: The full Unicode character set is not supported for this parameter.
- previousTrimSurfaceName (str) – the previous name of the trim surface feature. NOTE: The full Unicode character set is not supported for this parameter.
New in version NX7.5.0.
License requirements: None.
- trimPart (
Validate¶
-
DesignTrimToolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.