CornerDesignBuilder Class¶
-
class
NXOpen.Tooling.
CornerDesignBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.CornerDesignBuilder
, Corner Design is to provide tools to make corner.To create a new instance of this class, use
NXOpen.Tooling.CornerDesignCollection.CreateCornerDesignBuilder
Default values.
Property Value ChamferAngle.Value 45 CornerType Chamfer Offset.Value 1 (millimeters part), 0.1 (inches part) RadiusDia.Value 5 (millimeters part), 0.5 (inches part) SelectFrom Both New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ChamferAngle | Returns the chamfer angle. |
CornerType | Returns or sets the corner type |
Offset | Returns the offset. |
RadiusDia | Returns the corner radius. |
SelectCorner | Returns the selected corner. |
SelectEdge | Returns the selected edge. |
SelectFrom | Returns or sets the selection options. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the operation type of corner design. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CornerDesignBuilderCornerTypeOpt Enumeration | the corner types |
CornerDesignBuilderSelectFromOpt Enumeration | the object selection options. |
CornerDesignBuilderTypes Enumeration | The corner design type. |
Property Detail¶
ChamferAngle¶
-
CornerDesignBuilder.
ChamferAngle
¶ Returns the chamfer angle.
-------------------------------------
Getter Method
Signature
ChamferAngle()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
CornerType¶
-
CornerDesignBuilder.
CornerType
¶ Returns or sets the corner type
-------------------------------------
Getter Method
Signature
CornerType()
Returns: Return type: NXOpen.Tooling.CornerDesignBuilderCornerTypeOpt
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerType(cornerType)
Parameters: cornerType ( NXOpen.Tooling.CornerDesignBuilderCornerTypeOpt
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Offset¶
-
CornerDesignBuilder.
Offset
¶ Returns the offset.
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
RadiusDia¶
-
CornerDesignBuilder.
RadiusDia
¶ Returns the corner radius.
-------------------------------------
Getter Method
Signature
RadiusDia()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
SelectCorner¶
-
CornerDesignBuilder.
SelectCorner
¶ Returns the selected corner.
-------------------------------------
Getter Method
Signature
SelectCorner()
Returns: Return type: NXOpen.Features.SelectFeatureList
New in version NX8.0.0.
License requirements: None.
SelectEdge¶
-
CornerDesignBuilder.
SelectEdge
¶ Returns the selected edge.
-------------------------------------
Getter Method
Signature
SelectEdge()
Returns: Return type: NXOpen.SelectEdgeList
New in version NX8.0.0.
License requirements: None.
SelectFrom¶
-
CornerDesignBuilder.
SelectFrom
¶ Returns or sets the selection options.
-------------------------------------
Getter Method
Signature
SelectFrom()
Returns: Return type: NXOpen.Tooling.CornerDesignBuilderSelectFromOpt
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectFrom(selectFrom)
Parameters: selectFrom ( NXOpen.Tooling.CornerDesignBuilderSelectFromOpt
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Type¶
-
CornerDesignBuilder.
Type
¶ Returns or sets the operation type of corner design.
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Tooling.CornerDesignBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Tooling.CornerDesignBuilderTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
CornerDesignBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.