CoolingDefineChannelBuilderExtensionTypes Enumeration¶
NXOpen.Tooling.CoolingDefineChannelBuilder.ExtensionTypes is an alias for NXOpen.Tooling.CoolingDefineChannelBuilderExtensionTypes
-
class
NXOpen.Tooling.
CoolingDefineChannelBuilderExtensionTypes
¶ Bases:
object
The extension types of channel
Enum Members
Enum Member Enum Member Description NoExtension No extension AlongExtrusionDirection Extend channel to boundary body along the extrusion direction AlongReverseExtrusionDirection Extend channel to boundary body along the reverse extrusion direction AlongBothDirections Extend channel to boundary body along both direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-