CompDrawingBuilder Class¶
-
class
NXOpen.Tooling.
CompDrawingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.CompDrawingBuilder
which is used to create or edit the Component Drawing.To create a new instance of this class, use
NXOpen.Tooling.ToolingDrawingCollection.CreateComponentDrawingBuilder
Default values.
Property Value ComponentType All DrawingFilter None Filter Type IsKeepDrawingOpen 0 Margin 15 Projection FirstAngleProjection New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Component | Returns the component to create drawing. |
ComponentType | Returns or sets the component type in mold or die project assembly. |
DrawingFileNamingRule | Returns or sets the naming rule of drawing files. |
DrawingFilter | Returns or sets the drawing component drawing filter. |
DrawingSheetNamingRule | Returns or sets the naming rule of drawing sheets. |
Filter | Returns or sets the filter to select component for drawing. |
IsKeepDrawingOpen | Returns or sets the option whether to keep drawing open. |
Margin | Returns or sets the margin for user defined drawing template. |
MarginForView | Returns or sets the margin for view for user defined drawing template. |
Projection | Returns or sets the drawing projection angle. |
Tag | Returns the Tag for this object. |
WizardType | Returns or sets the wizard type attribute |
Methods¶
Method | Description |
---|---|
AddCompSheet | Add a new sheet to a component. |
Commit | Commits any edits that have been applied to the builder. |
CreateAll | Creates all drawings. |
CreateCompDrawing | Creates a drawing for a component |
CreateComponentDrawingCopyAttribute | Creates a drawing for a component and copy attribute to the drawing part |
CreateDrawing | Creates a drawing. |
DeleteCompDrawing | Deletes drawings in self-contained part or deletes a master model part with drawings |
DeleteCompSheet | Deletes a sheet from a component. |
DeleteDrawing | Deletes a drawing. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditCompDrawing | Edits a drawing in a component. |
EditDrawing | Edits a drawing. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitConstructor | Initializes the component drawing value. |
OpenCompDrawing | Opens a drawing in a component. |
OpenDrawing | Opens a drawing. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CompDrawingBuilderComponentTypeSelection Enumeration | Specifies the type of components. |
CompDrawingBuilderDrawingType Enumeration | Specifies the drawing type. |
CompDrawingBuilderFilterSelection Enumeration | Specifies the filter of components. |
CompDrawingBuilderProjectionType Enumeration | Specifies the project type. |
Property Detail¶
Component¶
-
CompDrawingBuilder.
Component
¶ Returns the component to create drawing.
-------------------------------------
Getter Method
Signature
Component()
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
ComponentType¶
-
CompDrawingBuilder.
ComponentType
¶ Returns or sets the component type in mold or die project assembly.
-------------------------------------
Getter Method
Signature
ComponentType()
Returns: Return type: NXOpen.Tooling.CompDrawingBuilderComponentTypeSelection
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComponentType(componentType)
Parameters: componentType ( NXOpen.Tooling.CompDrawingBuilderComponentTypeSelection
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DrawingFileNamingRule¶
-
CompDrawingBuilder.
DrawingFileNamingRule
¶ Returns or sets the naming rule of drawing files.
-------------------------------------
Getter Method
Signature
DrawingFileNamingRule()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingFileNamingRule(drawingFileNamingRule)
Parameters: drawingFileNamingRule (str) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DrawingFilter¶
-
CompDrawingBuilder.
DrawingFilter
¶ Returns or sets the drawing component drawing filter.
-------------------------------------
Getter Method
Signature
DrawingFilter()
Returns: Return type: NXOpen.Tooling.CompDrawingBuilderDrawingType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingFilter(drawingType)
Parameters: drawingType ( NXOpen.Tooling.CompDrawingBuilderDrawingType
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
DrawingSheetNamingRule¶
-
CompDrawingBuilder.
DrawingSheetNamingRule
¶ Returns or sets the naming rule of drawing sheets.
-------------------------------------
Getter Method
Signature
DrawingSheetNamingRule()
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawingSheetNamingRule(drawingSheetNamingRule)
Parameters: drawingSheetNamingRule (str) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Filter¶
-
CompDrawingBuilder.
Filter
¶ Returns or sets the filter to select component for drawing.
-------------------------------------
Getter Method
Signature
Filter()
Returns: Return type: NXOpen.Tooling.CompDrawingBuilderFilterSelection
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Filter(filter)
Parameters: filter ( NXOpen.Tooling.CompDrawingBuilderFilterSelection
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
IsKeepDrawingOpen¶
-
CompDrawingBuilder.
IsKeepDrawingOpen
¶ Returns or sets the option whether to keep drawing open.
-------------------------------------
Getter Method
Signature
IsKeepDrawingOpen()
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsKeepDrawingOpen(isKeepDrawingOpen)
Parameters: isKeepDrawingOpen (bool) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Margin¶
-
CompDrawingBuilder.
Margin
¶ Returns or sets the margin for user defined drawing template.
-------------------------------------
Getter Method
Signature
Margin()
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Margin(margin)
Parameters: margin (int) – New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MarginForView¶
-
CompDrawingBuilder.
MarginForView
¶ Returns or sets the margin for view for user defined drawing template.
-------------------------------------
Getter Method
Signature
MarginForView()
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MarginForView(marginForView)
Parameters: marginForView (float) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Projection¶
-
CompDrawingBuilder.
Projection
¶ Returns or sets the drawing projection angle.
-------------------------------------
Getter Method
Signature
Projection()
Returns: Return type: NXOpen.Tooling.CompDrawingBuilderProjectionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Projection(projection)
Parameters: projection ( NXOpen.Tooling.CompDrawingBuilderProjectionType
) –New in version NX8.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
WizardType¶
-
CompDrawingBuilder.
WizardType
¶ Returns or sets the wizard type attribute
-------------------------------------
Getter Method
Signature
WizardType()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WizardType(wizardType)
Parameters: wizardType (int) – New in version NX8.5.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
AddCompSheet¶
-
CompDrawingBuilder.
AddCompSheet
¶ Add a new sheet to a component.
Signature
AddCompSheet(component, componentPartName, drawingFileName, drawingName, templateName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
License requirements: None.
- component (
CreateAll¶
-
CompDrawingBuilder.
CreateAll
¶ Creates all drawings.
Signature
CreateAll()
New in version NX8.0.0.
License requirements: None.
CreateCompDrawing¶
-
CompDrawingBuilder.
CreateCompDrawing
¶ Creates a drawing for a component
Signature
CreateCompDrawing(component, componentPartName, drawingFileName, drawingName, templateName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Tooling.CompDrawingBuilder.CreateComponentDrawingCopyAttribute
instead.License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- component (
CreateComponentDrawingCopyAttribute¶
-
CompDrawingBuilder.
CreateComponentDrawingCopyAttribute
¶ Creates a drawing for a component and copy attribute to the drawing part
Signature
CreateComponentDrawingCopyAttribute(component, componentPartName, drawingFileName, drawingName, templateName, attributeTitles, attributeValues)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
- attributeTitles (list of str) – attribute titles NOTE: The full Unicode character set is not supported for this parameter.
- attributeValues (list of str) – attribute values NOTE: The full Unicode character set is not supported for this parameter.
New in version NX10.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
- component (
CreateDrawing¶
-
CompDrawingBuilder.
CreateDrawing
¶ Creates a drawing.
Signature
CreateDrawing(pName, dFile, dName, templateName)
Parameters: - pName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dFile (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Tooling.CompDrawingBuilder.CreateCompDrawing
instead.License requirements: None.
DeleteCompDrawing¶
-
CompDrawingBuilder.
DeleteCompDrawing
¶ Deletes drawings in self-contained part or deletes a master model part with drawings
Signature
DeleteCompDrawing(component, componentPartName, drawingFileName, drawingName, templateName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
License requirements: None.
- component (
DeleteCompSheet¶
-
CompDrawingBuilder.
DeleteCompSheet
¶ Deletes a sheet from a component.
Signature
DeleteCompSheet(component, componentPartName, drawingFileName, drawingName, templateName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
License requirements: None.
- component (
DeleteDrawing¶
-
CompDrawingBuilder.
DeleteDrawing
¶ Deletes a drawing.
Signature
DeleteDrawing(pName, dFile, dName, templateName)
Parameters: - pName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dFile (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Tooling.CompDrawingBuilder.DeleteCompDrawing
instead.License requirements: None.
EditCompDrawing¶
-
CompDrawingBuilder.
EditCompDrawing
¶ Edits a drawing in a component.
Signature
EditCompDrawing(component, componentPartName, drawingFileName, drawingName, templateName, oldSheetName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
- oldSheetName (str) – old sheet name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
License requirements: None.
- component (
EditDrawing¶
-
CompDrawingBuilder.
EditDrawing
¶ Edits a drawing.
Signature
EditDrawing(pName, dFile, dName, templateName)
Parameters: - pName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dFile (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Tooling.CompDrawingBuilder.EditCompDrawing
instead.License requirements: None.
InitConstructor¶
-
CompDrawingBuilder.
InitConstructor
¶ Initializes the component drawing value.
Signature
InitConstructor()
New in version NX8.0.0.
License requirements: None.
OpenCompDrawing¶
-
CompDrawingBuilder.
OpenCompDrawing
¶ Opens a drawing in a component.
Signature
OpenCompDrawing(component, componentPartName, drawingFileName, drawingName, templateName)
Parameters: - component (
NXOpen.NXObject
) – - componentPartName (str) – component part name NOTE: The full Unicode character set is not supported for this parameter.
- drawingFileName (str) – drawing file name NOTE: The full Unicode character set is not supported for this parameter.
- drawingName (str) – drawing name NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – template name NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.5.0.
License requirements: None.
- component (
OpenDrawing¶
-
CompDrawingBuilder.
OpenDrawing
¶ Opens a drawing.
Signature
OpenDrawing(pName, dFile, dName, templateName)
Parameters: - pName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dFile (str) – NOTE: The full Unicode character set is not supported for this parameter.
- dName (str) – NOTE: The full Unicode character set is not supported for this parameter.
- templateName (str) – NOTE: The full Unicode character set is not supported for this parameter.
New in version NX8.0.0.
Deprecated since version NX8.5.0: Use
NXOpen.Tooling.CompDrawingBuilder.OpenCompDrawing
instead.License requirements: None.
Validate¶
-
CompDrawingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.