ChannelAdjustBuilder Class¶
-
class
NXOpen.Tooling.
ChannelAdjustBuilder
¶ Bases:
NXOpen.Builder
The builder class for Channel Adjust which assists you to adjust the postion and the length of the channel.
To create a new instance of this class, use
NXOpen.Tooling.ChannelAdjustCollection.CreateChannelAdjustBuilder
Default values.
Property Value Distance.Value 0 (millimeters part), 0 (inches part) RepositionMethod Along New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AdjustMethod | Returns or sets the method for adjusting the cooling channels. |
AdjustVector | Returns or sets the vector specified for the adjust direction. |
Distance | Returns the distance between the channels and faces. |
ReferenceFace | Returns the reference faces for calculating the distance to the cooling channels. |
RepositionMethod | Returns or sets the method for moving the cooling channels. |
Tag | Returns the Tag for this object. |
TargetChannel | Returns the cooling channel to be adjusted. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetManipulatorOriginValue | Sets the manipulator origin. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ChannelAdjustBuilderAdjustType Enumeration | the adjust method. |
ChannelAdjustBuilderVectorMethod Enumeration | the vector adjust method. |
Property Detail¶
AdjustMethod¶
-
ChannelAdjustBuilder.
AdjustMethod
¶ Returns or sets the method for adjusting the cooling channels.
-------------------------------------
Getter Method
Signature
AdjustMethod()
Returns: Return type: NXOpen.Tooling.ChannelAdjustBuilderAdjustType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjustMethod(adjustMethod)
Parameters: adjustMethod ( NXOpen.Tooling.ChannelAdjustBuilderAdjustType
) –New in version NX7.5.0.
License requirements: None.
AdjustVector¶
-
ChannelAdjustBuilder.
AdjustVector
¶ Returns or sets the vector specified for the adjust direction.
-------------------------------------
Getter Method
Signature
AdjustVector()
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AdjustVector(adjustVector)
Parameters: adjustVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
Distance¶
-
ChannelAdjustBuilder.
Distance
¶ Returns the distance between the channels and faces.
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
ReferenceFace¶
-
ChannelAdjustBuilder.
ReferenceFace
¶ Returns the reference faces for calculating the distance to the cooling channels.
-------------------------------------
Getter Method
Signature
ReferenceFace()
Returns: Return type: NXOpen.ScCollector
New in version NX7.5.0.
License requirements: None.
RepositionMethod¶
-
ChannelAdjustBuilder.
RepositionMethod
¶ Returns or sets the method for moving the cooling channels.
-------------------------------------
Getter Method
Signature
RepositionMethod()
Returns: Return type: NXOpen.Tooling.ChannelAdjustBuilderVectorMethod
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RepositionMethod(repositionMethod)
Parameters: repositionMethod ( NXOpen.Tooling.ChannelAdjustBuilderVectorMethod
) –New in version NX7.5.0.
License requirements: None.
TargetChannel¶
-
ChannelAdjustBuilder.
TargetChannel
¶ Returns the cooling channel to be adjusted.
-------------------------------------
Getter Method
Signature
TargetChannel()
Returns: Return type: NXOpen.SelectBodyList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetManipulatorOriginValue¶
-
ChannelAdjustBuilder.
SetManipulatorOriginValue
¶ Sets the manipulator origin.
Signature
SetManipulatorOriginValue(moveOrigin)
Parameters: moveOrigin ( NXOpen.Point3d
) –New in version NX9.0.2.
License requirements: ug_mold_design (“UG MOLD”)
Validate¶
-
ChannelAdjustBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.