BlankLayoutBuilderTypes Enumeration¶
NXOpen.Tooling.BlankLayoutBuilder.Types is an alias for NXOpen.Tooling.BlankLayoutBuilderTypes
-
class
NXOpen.Tooling.
BlankLayoutBuilderTypes
¶ Bases:
object
Specifies the option of blank layout type.
Enum Members
Enum Member Enum Member Description CreateLayout the type of create blank layoutAddBlank the type of add multiple blankCopyBlank the type of copy blankRemoveBlank the type of remove blankSetBasePoint the type of set the base point of the blankFlipBlank the type of flip blank-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-