BlankLayoutBuilderSideWebOption Enumeration¶
NXOpen.Tooling.BlankLayoutBuilder.SideWebOption is an alias for NXOpen.Tooling.BlankLayoutBuilderSideWebOption
-
class
NXOpen.Tooling.
BlankLayoutBuilderSideWebOption
¶ Bases:
object
Specifies the option of side webs type.
Enum Members
Enum Member Enum Member Description Average the side webs type of averageBottom the side webs type of bottomTop the side webs type of top-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-