BlankGeneratorBuilderTypes Enumeration¶
NXOpen.Tooling.BlankGeneratorBuilder.Types is an alias for NXOpen.Tooling.BlankGeneratorBuilderTypes
-
class
NXOpen.Tooling.
BlankGeneratorBuilderTypes
¶ Bases:
object
Specifies the option of blank generator operation type.
Enum Members
Enum Member Enum Member Description CreateBlank Create a blank.EditBlank Edit a blank.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-