AddReusableFeatureCollection Class¶
-
class
NXOpen.Tooling.
AddReusableFeatureCollection
¶ Bases:
object
Represents a collection of AddReusableFeature
To obtain an instance of this class, refer to
NXOpen.Tooling.ToolingManager
New in version NX7.5.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates a AddReusableFeature builder @return Add Reusable Feature Builder |
Structs¶
AddReusableFeatureCollectionInputData_Struct Struct | Defines the input data of AddReusableFeatureBuilder |
Method Detail¶
CreateBuilder¶
-
AddReusableFeatureCollection.
CreateBuilder
¶ Creates a AddReusableFeature builder
Signature
CreateBuilder(inputData)
Parameters: inputData ( NXOpen.Tooling.AddReusableFeatureCollectionInputData_Struct
) – Input dataReturns: Add Reusable Feature Builder Return type: NXOpen.Tooling.AddReusableFeatureBuilder
New in version NX7.5.0.
License requirements: None.