TableEditorDefaultDataProvider Class¶
-
class
NXOpen.
TableEditorDefaultDataProvider
¶ Bases:
NXOpen.Builder
,NXOpen.ITableEditorDataProvider
Provides basic data for a Table Editor block.
To create a new instance of this class, use
NXOpen.Session.CreateTableEditorDefaultDataProvider
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ColumnCount | Returns or sets the number of columns in the table |
RowCount | Returns or sets the number of rows in the table |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetString | Gets the string data at a particular location in the table @return the string data at the row and column specified |
SetString | Sets string data at a particular location in the table. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ColumnCount¶
-
TableEditorDefaultDataProvider.
ColumnCount
¶ Returns or sets the number of columns in the table
-------------------------------------
Getter Method
Signature
ColumnCount()
Returns: the number of columns in the table Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ColumnCount(columnCount)
Parameters: columnCount (int) – the number of columns in the table New in version NX10.0.0.
License requirements: None.
RowCount¶
-
TableEditorDefaultDataProvider.
RowCount
¶ Returns or sets the number of rows in the table
-------------------------------------
Getter Method
Signature
RowCount()
Returns: the number of rows in the table Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RowCount(rowCount)
Parameters: rowCount (int) – the number of columns in the table New in version NX10.0.0.
License requirements: None.
Method Detail¶
GetString¶
-
TableEditorDefaultDataProvider.
GetString
¶ Gets the string data at a particular location in the table
Signature
GetString(row, column)
Parameters: - row (int) – the rows to query
- column (int) – the column to query
Returns: the string data at the row and column specified
Return type: str
New in version NX10.0.0.
License requirements: None.
SetString¶
-
TableEditorDefaultDataProvider.
SetString
¶ Overloaded method SetString
SetString(rows, column, stringData)
SetString(rows, column, stringData)
-------------------------------------
Sets string data at a particular location in the table.
Signature
SetString(rows, column, stringData)
Parameters: - rows (int) – the row to set
- column (int) – the column to set
- stringData (str) – the string data to set
Returns: whether or not the data was successfully set.
Return type: bool
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Sets string data on a range of table cells in a specified column. Returns whether any data was successfully set.
Signature
SetString(rows, column, stringData)
Parameters: - rows (list of int) – the rows to set
- column (int) – the column to be set
- stringData (str) – the string data to set
Returns: whether or not the data was successfully set.
Return type: bool
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Validate¶
-
TableEditorDefaultDataProvider.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.