SketchQuickExtendBuilder Class¶
-
class
NXOpen.
SketchQuickExtendBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchQuickExtendBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateQuickExtendBuilder
Default values.
Property Value ExtendBound True New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BoundaryCurves | Returns the boundary curves |
BoundaryObjects | Returns the boundary objects |
ExtendBound | Returns or sets the flag to control the ability to extend to extension of the boundary |
ExtendedCurves | Returns the extended curves |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BoundaryCurves¶
-
SketchQuickExtendBuilder.
BoundaryCurves
¶ Returns the boundary curves
-------------------------------------
Getter Method
Signature
BoundaryCurves()
Returns: Return type: NXOpen.SelectCurveList
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.SketchQuickExtendBuilder.BoundaryObjects
instead.License requirements: None.
BoundaryObjects¶
-
SketchQuickExtendBuilder.
BoundaryObjects
¶ Returns the boundary objects
-------------------------------------
Getter Method
Signature
BoundaryObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
ExtendBound¶
-
SketchQuickExtendBuilder.
ExtendBound
¶ Returns or sets the flag to control the ability to extend to extension of the boundary
-------------------------------------
Getter Method
Signature
ExtendBound()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendBound(extendBound)
Parameters: extendBound (bool) – New in version NX6.0.0.
License requirements: None.
ExtendedCurves¶
-
SketchQuickExtendBuilder.
ExtendedCurves
¶ Returns the extended curves
-------------------------------------
Getter Method
Signature
ExtendedCurves()
Returns: Return type: NXOpen.SelectCurveList
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SketchQuickExtendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.