SketchPatternBuilder Class¶
-
class
NXOpen.
SketchPatternBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchPatternBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchPatternBuilder
Default values.
Property Value CreateSpacingExp True LockOrientation True PatternService.AlongPathDefinition.XOnPathSpacing.NCopies.Value 2 PatternService.AlongPathDefinition.XOnPathSpacing.SpaceType Offset PatternService.AlongPathDefinition.XPathOption Offset PatternService.AlongPathDefinition.YDirectionOption Section PatternService.AlongPathDefinition.YOnPathSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YPathOption Offset PatternService.AlongPathDefinition.YSpacing.NCopies.Value 1 PatternService.AlongPathDefinition.YSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.AlongPathDefinition.YSpacing.SpaceType Offset PatternService.AlongPathDefinition.YSpacing.SpanDistance.Value 100 (millimeters part), 10 (inches part) PatternService.CircularDefinition.AngularSpacing.NCopies.Value 12 PatternService.CircularDefinition.AngularSpacing.PitchAngle.Value 30 PatternService.CircularDefinition.AngularSpacing.PitchDistance.Value 10 (millimeters part), 1 (inches part) PatternService.CircularDefinition.AngularSpacing.SpaceType Offset PatternService.CircularDefinition.AngularSpacing.SpanAngle.Value 360 (millimeters part), 360 (inches part) PatternService.CircularDefinition.AngularSpacing.UsePitchOption Angle PatternService.CircularDefinition.CreateLastStaggered true PatternService.CircularDefinition.HorizontalRef.RotationAngle.Value 0 (millimeters part), 0 (inches part) PatternService.CircularDefinition.IncludeSeedToggle true PatternService.CircularDefinition.RadialSpacing.NCopies.Value 1 PatternService.CircularDefinition.StaggerType None PatternService.HelixDefinition.AnglePitch.Value 30 PatternService.HelixDefinition.CountOfInstances.Value 6 PatternService.HelixDefinition.DirectionType Righthand PatternService.HelixDefinition.DistancePitch.Value 10 (millimeters part), 0.4 (inches part) PatternService.HelixDefinition.HelixPitch.Value 50 (millimeters part), 2 (inches part) PatternService.HelixDefinition.HelixSpan.Value 100 (millimeters part), 4 (inches part) PatternService.HelixDefinition.NumberOfTurns.Value 2 PatternService.HelixDefinition.SizeOption CountAngleDistance PatternService.PatternFill.FillMargin.Value 0 (millimeters part), 0 (inches part) PatternService.PatternFill.FillOptions None PatternService.PatternFill.SimplifiedBoundaryToggle False PatternService.PatternOrientation.AlongOrientationOption NormalToPath PatternService.PatternOrientation.CircularOrientationOption FollowPattern PatternService.PatternOrientation.FollowFaceProjDirOption PatternPlaneNormal PatternService.PatternOrientation.GeneralOrientationOption Fixed PatternService.PatternOrientation.HelixOrientationOption FollowPattern PatternService.PatternOrientation.LinearOrientationOption Fixed PatternService.PatternOrientation.MirrorOrientationOption FollowPattern PatternService.PatternOrientation.OrientationOption Fixed PatternService.PatternOrientation.PolygonOrientationOption FollowPattern PatternService.PatternOrientation.SpiralOrientationOption FollowPattern PatternService.PatternType Linear PatternService.PolygonDefinition.NumberOfSides.Value 6 PatternService.PolygonDefinition.PolygonSizeOption Inscribed PatternService.PolygonDefinition.PolygonSpacing.NCopies.Value 4 PatternService.PolygonDefinition.PolygonSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.PolygonSpacing.SpaceType Offset PatternService.PolygonDefinition.PolygonSpacing.SpanAngle.Value 360 PatternService.PolygonDefinition.RadialSpacing.NCopies.Value 1 PatternService.PolygonDefinition.RadialSpacing.PitchDistance.Value 25 (millimeters part), 1 (inches part) PatternService.PolygonDefinition.RadialSpacing.SpanDistance.Value 100 (millimeters part), 4 (inches part) PatternService.RectangularDefinition.CreateLastStaggered true PatternService.RectangularDefinition.SimplifiedLayoutType Square PatternService.RectangularDefinition.StaggerType None PatternService.RectangularDefinition.XSpacing.NCopies.Value 2 PatternService.RectangularDefinition.YSpacing.NCopies.Value 1 PatternService.SpiralDefinition.DirectionType Lefthand PatternService.SpiralDefinition.NumberOfTurns.Value 1 (millimeters part), 1 (inches part) PatternService.SpiralDefinition.RadialPitch.Value 50 (millimeters part), 2 (inches part) PatternService.SpiralDefinition.SizeSpiralType NumberOfTurns PatternService.SpiralDefinition.TotalAngle.Value 360 (millimeters part), 360 (inches part) New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
CreateSpacingExp | Returns or sets the flag to indicate if a spacing expression needs to be created |
LockOrientation | Returns or sets the flag to indicate if a spacing expression needs to be created |
PatternService | Returns the pattern service |
Section | Returns the pattern section |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetEndConstraint | This function removes end constraint from the given pattern |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateCopies | This function updates the pattern constraint with the number of copies set in the builder |
UpdateInputSection | This function updates the pattern constraint according to the data set in pattern section |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CreateSpacingExp¶
-
SketchPatternBuilder.
CreateSpacingExp
¶ Returns or sets the flag to indicate if a spacing expression needs to be created
-------------------------------------
Getter Method
Signature
CreateSpacingExp()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateSpacingExp(createSpacingExp)
Parameters: createSpacingExp (bool) – New in version NX7.5.0.
License requirements: None.
LockOrientation¶
-
SketchPatternBuilder.
LockOrientation
¶ Returns or sets the flag to indicate if a spacing expression needs to be created
-------------------------------------
Getter Method
Signature
LockOrientation()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockOrientation(lockOrientation)
Parameters: lockOrientation (bool) – New in version NX7.5.0.
License requirements: None.
PatternService¶
-
SketchPatternBuilder.
PatternService
¶ Returns the pattern service
-------------------------------------
Getter Method
Signature
PatternService()
Returns: Parttern Service object Return type: NXOpen.GeometricUtilities.PatternDefinition
New in version NX7.5.0.
License requirements: None.
Section¶
-
SketchPatternBuilder.
Section
¶ Returns the pattern section
-------------------------------------
Getter Method
Signature
Section()
Returns: Section object Return type: NXOpen.Section
New in version NX7.5.0.
License requirements: None.
Method Detail¶
SetEndConstraint¶
-
SketchPatternBuilder.
SetEndConstraint
¶ This function removes end constraint from the given pattern
Signature
SetEndConstraint(parent, inx, isStart, constraint)
Parameters: - parent (
NXOpen.NXObject
) – Parent object in base chain - inx (int) – Index of the pattern - starts from 0
- isStart (bool) – TRUE, if we want to remove the start end con
- constraint (bool) – TRUE to add the con, false to remove
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- parent (
UpdateCopies¶
-
SketchPatternBuilder.
UpdateCopies
¶ This function updates the pattern constraint with the number of copies set in the builder
Signature
UpdateCopies()
New in version NX8.5.0.
License requirements: None.
UpdateInputSection¶
-
SketchPatternBuilder.
UpdateInputSection
¶ This function updates the pattern constraint according to the data set in pattern section
Signature
UpdateInputSection()
New in version NX8.5.0.
License requirements: None.
Validate¶
-
SketchPatternBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.