SketchIntersectionCurveBuilder Class¶
-
class
NXOpen.
SketchIntersectionCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.SketchIntersectionCurve
builderTo obtain an instance of this class use
NXOpen.SketchCollection.CreateIntersectionCurveBuilder
.Default values.
Property Value CurveFitMethod.FitOption Cubic CurveFitMethod.MaximumDegree 7 CurveFitMethod.MaximumSegments 1 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngleTolerance | Returns or sets the angular tolerance |
CurveFitMethod | Returns the curve fit method |
DistanceTolerance | Returns or sets the distance tolerance |
FaceCollector | Returns the faces to intersect |
IgnoreHoles | Returns or sets the ignore holes option |
JoinCurves | Returns or sets the join curves option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AlternateSolution | Method to get the alternate solution corresponding to solutionIndex |
CollectorUpdated | This method needs to be called whenever the number of faces to intersect changes |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CurveFitMethodUpdated | This method needs to be called whenever the curve fit options changes |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AngleTolerance¶
-
SketchIntersectionCurveBuilder.
AngleTolerance
¶ Returns or sets the angular tolerance
-------------------------------------
Getter Method
Signature
AngleTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngleTolerance(angleTolerance)
Parameters: angleTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CurveFitMethod¶
-
SketchIntersectionCurveBuilder.
CurveFitMethod
¶ Returns the curve fit method
-------------------------------------
Getter Method
Signature
CurveFitMethod()
Returns: curve fit option Return type: NXOpen.GeometricUtilities.CurveFitOptions
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
DistanceTolerance¶
-
SketchIntersectionCurveBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance
-------------------------------------
Getter Method
Signature
DistanceTolerance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance(distanceTolerance)
Parameters: distanceTolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
FaceCollector¶
-
SketchIntersectionCurveBuilder.
FaceCollector
¶ Returns the faces to intersect
-------------------------------------
Getter Method
Signature
FaceCollector()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
IgnoreHoles¶
-
SketchIntersectionCurveBuilder.
IgnoreHoles
¶ Returns or sets the ignore holes option
-------------------------------------
Getter Method
Signature
IgnoreHoles()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IgnoreHoles(ignoreHoles)
Parameters: ignoreHoles (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
JoinCurves¶
-
SketchIntersectionCurveBuilder.
JoinCurves
¶ Returns or sets the join curves option
-------------------------------------
Getter Method
Signature
JoinCurves()
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
JoinCurves(joinCurves)
Parameters: joinCurves (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Method Detail¶
AlternateSolution¶
-
SketchIntersectionCurveBuilder.
AlternateSolution
¶ Method to get the alternate solution corresponding to solutionIndex
Signature
AlternateSolution(solutionIndex)
Parameters: solutionIndex (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CollectorUpdated¶
-
SketchIntersectionCurveBuilder.
CollectorUpdated
¶ This method needs to be called whenever the number of faces to intersect changes
Signature
CollectorUpdated()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CurveFitMethodUpdated¶
-
SketchIntersectionCurveBuilder.
CurveFitMethodUpdated
¶ This method needs to be called whenever the curve fit options changes
Signature
CurveFitMethodUpdated()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
Validate¶
-
SketchIntersectionCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.